Other Parts Discussed in Thread: AM3517
All:
One of our board houses has hit a problem with the MMC2 port on AM3517 that cannot resolve. More details are below:
We are almost ready to launch AM3517 module but encounter a serious bug that we cannot even get working on the Logic demoboard and therefore want to check with TI if our demoboard is broken or that this is a known AM3517 bug.
The description of problem is as follow which already be sent to your TI Taiwan FAE but without response. (maybe he is just waiting for US response but we will value some initial feedback in order to avoid a large delay on our developmentcycle).
***quote engineer***
We got a problem on am3517 about mmc2 port, we tried to use the mmc2 port but without success,
the mmc2 can output cmd/clk signal but all sdcard/sdio-card has no response at all, no data output from data-pins. (the same routine on mmc1 is working fine)
both kernel and u-boot cannot working.
***end quote engineer***
As you can see above we have issues with the MMC2 port not only on our board but also on the Logic EVM board and want to verify if on the original EVM's this is working or not. If it's working. Can you be so kind to send us the U-Boot and kernel that is used on the board in order for our engineers to verify operation on our side.
As a final note. Our schematics is straight 100% copy from the EVM on this part. No modifications there. On the MMC2 we have connected a WIFI module (TI chips made by JOR-JIN a TI customer as well and introduced to us by TI Taiwan).
Thank you in advance so much for your help.
Kind regards,
Marcel vandenHeuvel
TechNexion Ltd.
17F-1, No. 16, Jian Ba Road
Chung Ho City, 235, Taipei, Taiwan
phone : +886-2-82273585
mobile : +886-988 112650
fax : +886-2-82273590
email : marcel@technexion.com