Part Number: AM5728
Other Parts Discussed in Thread: DRA752, TPD12S015, TMP102, TLV320AIC3104, PMP
Tool/software: Linux
Hello,
we connected a custom adv7842 board with the vip on the evm5728.
The adv7842 video device driver included in the kernel 4.4.19 doesn't support the device tree. So I made the following changes in the probe function:
1. Set platform data manually (could later be retrieved from device tree)
2. Call v4l2_async_register_subdev(sd) at end of probe function
No other changes are made in the driver.
static int adv7842_probe(struct i2c_client *client,
const struct i2c_device_id *id)
{
struct adv7842_state *state;
static const struct v4l2_dv_timings cea640x480 =
V4L2_DV_BT_CEA_640X480P59_94;
struct adv7842_platform_data *pdata;
struct v4l2_ctrl_handler *hdl;
struct v4l2_subdev *sd;
u16 rev;
int err;
/* Check if the adapter supports the needed features */
if (!i2c_check_functionality(client->adapter, I2C_FUNC_SMBUS_BYTE_DATA))
return -EIO;
v4l_dbg(1, debug, client, "detecting adv7842 client on address 0x%x\n",
client->addr << 1);
/****** NEW *******/
struct adv7842_platform_data adv7842_pdata = {
.disable_pwrdnb = 1,
.ain_sel = ADV7842_AIN1_2_3_NC_SYNC_1_2,
.bus_order = ADV7842_BUS_ORDER_RBG,
.op_format_mode_sel = ADV7842_OP_FORMAT_MODE0,
.blank_data = 1,
.op_656_range = 1,
.dr_str_data = 3,
.dr_str_clk = 3,
.dr_str_sync = 3,
.mode = ADV7842_MODE_HDMI,
.hdmi_free_run_enable = 1,
.vid_std_select = ADV7842_HDMI_COMP_VID_STD_HD_1250P,
.i2c_sdp_io = 0x4a,
.i2c_sdp = 0x48,
.i2c_cp = 0x22,
.i2c_vdp = 0x24,
.i2c_afe = 0x26,
.i2c_hdmi = 0x34,
.i2c_repeater = 0x32,
.i2c_edid = 0x36,
.i2c_infoframe = 0x3e,
.i2c_cec = 0x40,
.i2c_avlink = 0x42,
};
pdata = &adv7842_pdata;
/***** END NEW *****/
state = devm_kzalloc(&client->dev, sizeof(struct adv7842_state), GFP_KERNEL);
if (!state) {
v4l_err(client, "Could not allocate adv7842_state memory!\n");
return -ENOMEM;
}
/* platform data */
state->pdata = *pdata;
state->timings = cea640x480;
state->format = adv7842_format_info(state, MEDIA_BUS_FMT_YUYV8_2X8);
sd = &state->sd;
v4l2_i2c_subdev_init(sd, client, &adv7842_ops);
sd->flags |= V4L2_SUBDEV_FL_HAS_DEVNODE | V4L2_SUBDEV_FL_HAS_EVENTS;
state->mode = pdata->mode;
state->hdmi_port_a = pdata->input == ADV7842_SELECT_HDMI_PORT_A;
state->restart_stdi_once = true;
/* i2c access to adv7842? */
rev = adv_smbus_read_byte_data_check(client, 0xea, true) << 8 |
adv_smbus_read_byte_data_check(client, 0xeb, true);
if (rev != 0x2012) {
v4l2_info(sd, "got rev=0x%04x on first read attempt\n", rev);
rev = adv_smbus_read_byte_data_check(client, 0xea, true) << 8 |
adv_smbus_read_byte_data_check(client, 0xeb, true);
}
if (rev != 0x2012) {
v4l2_info(sd, "not an adv7842 on address 0x%x (rev=0x%04x)\n",
client->addr << 1, rev);
return -ENODEV;
}
if (pdata->chip_reset)
main_reset(sd);
/* control handlers */
hdl = &state->hdl;
v4l2_ctrl_handler_init(hdl, 6);
/* add in ascending ID order */
v4l2_ctrl_new_std(hdl, &adv7842_ctrl_ops,
V4L2_CID_BRIGHTNESS, -128, 127, 1, 0);
v4l2_ctrl_new_std(hdl, &adv7842_ctrl_ops,
V4L2_CID_CONTRAST, 0, 255, 1, 128);
v4l2_ctrl_new_std(hdl, &adv7842_ctrl_ops,
V4L2_CID_SATURATION, 0, 255, 1, 128);
v4l2_ctrl_new_std(hdl, &adv7842_ctrl_ops,
V4L2_CID_HUE, 0, 128, 1, 0);
/* custom controls */
state->detect_tx_5v_ctrl = v4l2_ctrl_new_std(hdl, NULL,
V4L2_CID_DV_RX_POWER_PRESENT, 0, 3, 0, 0);
state->analog_sampling_phase_ctrl = v4l2_ctrl_new_custom(hdl,
&adv7842_ctrl_analog_sampling_phase, NULL);
state->free_run_color_ctrl_manual = v4l2_ctrl_new_custom(hdl,
&adv7842_ctrl_free_run_color_manual, NULL);
state->free_run_color_ctrl = v4l2_ctrl_new_custom(hdl,
&adv7842_ctrl_free_run_color, NULL);
state->rgb_quantization_range_ctrl =
v4l2_ctrl_new_std_menu(hdl, &adv7842_ctrl_ops,
V4L2_CID_DV_RX_RGB_RANGE, V4L2_DV_RGB_RANGE_FULL,
0, V4L2_DV_RGB_RANGE_AUTO);
sd->ctrl_handler = hdl;
if (hdl->error) {
err = hdl->error;
goto err_hdl;
}
state->detect_tx_5v_ctrl->is_private = true;
state->rgb_quantization_range_ctrl->is_private = true;
state->analog_sampling_phase_ctrl->is_private = true;
state->free_run_color_ctrl_manual->is_private = true;
state->free_run_color_ctrl->is_private = true;
if (adv7842_s_detect_tx_5v_ctrl(sd)) {
err = -ENODEV;
goto err_hdl;
}
if (adv7842_register_clients(sd) < 0) {
err = -ENOMEM;
v4l2_err(sd, "failed to create all i2c clients\n");
goto err_i2c;
}
/* work queues */
state->work_queues = create_singlethread_workqueue(client->name);
if (!state->work_queues) {
v4l2_err(sd, "Could not create work queue\n");
err = -ENOMEM;
goto err_i2c;
}
INIT_DELAYED_WORK(&state->delayed_work_enable_hotplug,
adv7842_delayed_work_enable_hotplug);
state->pad.flags = MEDIA_PAD_FL_SOURCE;
err = media_entity_init(&sd->entity, 1, &state->pad, 0);
if (err)
goto err_work_queues;
err = adv7842_core_init(sd);
if (err)
goto err_entity;
v4l2_info(sd, "%s found @ 0x%x (%s)\n", client->name,
client->addr << 1, client->adapter->name);
/***** NEW ******/
err = v4l2_async_register_subdev(sd);
if (err)
goto err_entity;
/**** END NEW *****/
return 0;
err_entity:
media_entity_cleanup(&sd->entity);
err_work_queues:
cancel_delayed_work(&state->delayed_work_enable_hotplug);
destroy_workqueue(state->work_queues);
err_i2c:
adv7842_unregister_clients(sd);
err_hdl:
v4l2_ctrl_handler_free(hdl);
return err;
}
Additionally I use the following device tree entries:
&i2c5 {
status = "okay";
clock-frequency = <400000>;
adv7842@20 {
compatible = "adi,adv7842";
reg = <0x20>;
port {
adv7842_1: endpoint {
remote-endpoint = <&vin3a>;
};
};
};
};
&vin3a {
status = "okay";
endpoint {
slave-mode;
remote-endpoint = <&adv7842_1>;
};
};
dmesg shows the following output:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.19-gdb0b54cdad (marc@marc-VirtualBox) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #57 SMP PREEMPT Wed Jun 21 11:30:40 CEST 2017
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM572x EVM Rev A3
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier
[ 0.000000] On node 0 totalpages: 474368
[ 0.000000] free_area_init_node: node 0, pgdat c096afc0, node_mem_map eeda2000
[ 0.000000] DMA zone: 1728 pages used for memmap
[ 0.000000] DMA zone: 0 pages reserved
[ 0.000000] DMA zone: 147456 pages, LIFO batch:31
[ 0.000000] HighMem zone: 326912 pages, LIFO batch:31
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eed30000 s14848 r8192 d22016 u45056
[ 0.000000] pcpu-alloc: s14848 r8192 d22016 u45056 alloc=11*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 472640
[ 0.000000] Kernel command line: console=ttyO2,115200n8 root=/dev/nfs nfsroot=192.168.3.221:/home/marc/ti-processor-sdk-linux-am57xx-evm-03.01.00.06/targetNFS,nolock,v3,tcp,rsize=4096,wsize=4096 rw ip=dhcp
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1680704K/1897472K available (6535K kernel code, 358K rwdata, 2392K rodata, 332K init, 289K bss, 28352K reserved, 188416K cma-reserved, 1283072K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc08c004c (8929 kB)
.init : 0xc08c1000 - 0xc0914000 ( 332 kB)
.data : 0xc0914000 - 0xc096dab0 ( 359 kB)
.bss : 0xc096f000 - 0xc09b76c0 ( 290 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000015] Switching to timer-based delay loop, resolution 162ns
[ 0.000329] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000337] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000761] Console: colour dummy device 80x30
[ 0.000778] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2'
[ 0.000784] This ensures that you still see kernel messages. Please
[ 0.000790] update your kernel commandline.
[ 0.000803] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000816] pid_max: default: 32768 minimum: 301
[ 0.000909] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000919] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001454] Initializing cgroup subsys io
[ 0.001471] Initializing cgroup subsys memory
[ 0.001495] Initializing cgroup subsys devices
[ 0.001508] Initializing cgroup subsys freezer
[ 0.001519] Initializing cgroup subsys perf_event
[ 0.001530] Initializing cgroup subsys pids
[ 0.001555] CPU: Testing write buffer coherency: ok
[ 0.001754] /cpus/cpu@0 missing clock-frequency property
[ 0.001769] /cpus/cpu@1 missing clock-frequency property
[ 0.001779] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001813] Setting up static identity map for 0x800082c0 - 0x80008318
[ 0.080082] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080140] Brought up 2 CPUs
[ 0.080153] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080159] CPU: All CPU(s) started in SVC mode.
[ 0.080528] devtmpfs: initialized
[ 0.108546] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.109516] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.314064] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.317960] pinctrl core: initialized pinctrl subsystem
[ 0.318803] NET: Registered protocol family 16
[ 0.319715] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350239] cpuidle: using governor ladder
[ 0.380263] cpuidle: using governor menu
[ 0.388326] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.388865] OMAP GPIO hardware version 0.1
[ 0.389531] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.390454] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.391332] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.392180] gpiochip_add: registered GPIOs 128 to 159 on device: gpio
[ 0.393030] gpiochip_add: registered GPIOs 160 to 191 on device: gpio
[ 0.393875] gpiochip_add: registered GPIOs 192 to 223 on device: gpio
[ 0.394725] gpiochip_add: registered GPIOs 224 to 255 on device: gpio
[ 0.395336] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.420989] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.420999] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.421461] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.421470] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.422032] OMAP DMA hardware revision 0.0
[ 0.454489] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.455621] edma 43300000.edma: memcpy is disabled
[ 0.460417] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.460820] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-vdd_3v3[0]'
[ 0.461035] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator-aic_dvdd[0]'
[ 0.461272] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator-vtt[0]' - status (0)
[ 0.461533] of_get_named_gpiod_flags: parsed 'gpio' property of node '/fixedregulator-mmcwl[0]' - status (0)
[ 0.464392] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.464573] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.464725] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.464877] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.465150] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.465342] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.468267] palmas 0-0058: Irq flag is 0x00000008
[ 0.481959] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
[ 0.563557] gpiochip_find_base: found new base at 504
[ 0.563660] gpiochip_add: registered GPIOs 504 to 511 on device: 48070000.i2c:tps659038@58:tps659038_gpio
[ 0.564083] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.564584] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.565156] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
[ 0.565364] media: Linux media interface: v0.10
[ 0.565415] Linux video capture interface: v2.00
[ 0.565456] pps_core: LinuxPPS API ver. 1 registered
[ 0.565462] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.565486] PTP clock support registered
[ 0.565538] EDAC MC: Ver: 3.0.0
[ 0.566279] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.566571] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.566862] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.567143] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.567467] Advanced Linux Sound Architecture Driver Initialized.
[ 0.568272] clocksource: Switched to clocksource arch_sys_counter
[ 0.579271] NET: Registered protocol family 2
[ 0.579763] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.579826] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.579951] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.580000] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.580031] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.580170] NET: Registered protocol family 1
[ 0.580442] RPC: Registered named UNIX socket transport module.
[ 0.580451] RPC: Registered udp transport module.
[ 0.580458] RPC: Registered tcp transport module.
[ 0.580464] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.580481] PCI: CLS 0 bytes, default 64
[ 0.581492] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.583889] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.591664] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.592294] NFS: Registering the id_resolver key type
[ 0.592320] Key type id_resolver registered
[ 0.592328] Key type id_legacy registered
[ 0.592386] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.594344] bounce: pool size: 64 pages
[ 0.594493] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.594508] io scheduler noop registered
[ 0.594521] io scheduler deadline registered
[ 0.594556] io scheduler cfq registered (default)
[ 0.599544] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.603038] dra7-pcie 51000000.pcie: GPIO lookup for consumer (null)
[ 0.603050] dra7-pcie 51000000.pcie: using device tree for GPIO lookup
[ 0.603081] of_get_named_gpiod_flags: parsed 'gpios' property of node '/ocp/axi@0/pcie@51000000[0]' - status (0)
[ 0.603194] PCI host bridge /ocp/axi@0/pcie@51000000 ranges:
[ 0.603205] No bus range found for /ocp/axi@0/pcie@51000000, using [bus 00-ff]
[ 0.603238] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.603258] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.633566] dra7-pcie 51000000.pcie: link is not up
[ 0.633741] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 0.633753] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.633763] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.633772] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.633805] pci 0000:00:00.0: [104c:8888] type 01 class 0x060400
[ 0.633848] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
[ 0.633870] pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x0000ffff]
[ 0.633938] pci 0000:00:00.0: supports D1
[ 0.633948] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[ 0.634185] PCI: bus0: Fast back to back transfers disabled
[ 0.634309] PCI: bus1: Fast back to back transfers enabled
[ 0.634358] irq: no irq domain found for /ocp/axi@0/pcie@51000000/interrupt-controller !
[ 0.634394] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.634408] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.634421] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.634641] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.634654] pcie_pme 0000:00:00.0:pcie01: service driver pcie_pme loaded
[ 0.634772] aer 0000:00:00.0:pcie02: service driver aer loaded
[ 0.635879] pwm-backlight backlight: GPIO lookup for consumer enable
[ 0.635889] pwm-backlight backlight: using device tree for GPIO lookup
[ 0.635898] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[ 0.635907] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[ 0.635915] pwm-backlight backlight: using lookup tables for GPIO lookup
[ 0.635924] pwm-backlight backlight: lookup for GPIO enable failed
[ 0.635956] backlight supply power not found, using dummy regulator
[ 0.695588] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.698963] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.660478] console [ttyS2] enabled
[ 1.664807] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.674902] [drm] Initialized drm 1.1.0 20060810
[ 1.681559] OMAP DSS rev 6.1
[ 1.685332] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 1.693809] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
[ 1.702773] tpd12s015 encoder: GPIO lookup for consumer (null)
[ 1.702784] tpd12s015 encoder: using device tree for GPIO lookup
[ 1.702814] of_get_named_gpiod_flags: parsed 'gpios' property of node '/encoder[0]' - status (0)
[ 1.702831] tpd12s015 encoder: GPIO lookup for consumer (null)
[ 1.702840] tpd12s015 encoder: using device tree for GPIO lookup
[ 1.702877] of_get_named_gpiod_flags: parsed 'gpios' property of node '/encoder[1]' - status (0)
[ 1.702891] tpd12s015 encoder: GPIO lookup for consumer (null)
[ 1.702898] tpd12s015 encoder: using device tree for GPIO lookup
[ 1.702949] of_get_named_gpiod_flags: parsed 'gpios' property of node '/encoder[2]' - status (0)
[ 1.703503] of_get_named_gpiod_flags: can't parse 'hpd-gpios' property of node '/connector[0]'
[ 1.703792] panel-dpi display: GPIO lookup for consumer enable
[ 1.703802] panel-dpi display: using device tree for GPIO lookup
[ 1.703830] of_get_named_gpiod_flags: parsed 'enable-gpios' property of node '/display[0]' - status (0)
[ 1.710000] loop: module loaded
[ 1.715935] libphy: Fixed MDIO Bus: probed
[ 1.768306] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.774429] davinci_mdio 48485000.mdio: detected phy mask fffffff9
[ 1.784917] libphy: 48485000.mdio: probed
[ 1.788989] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
[ 1.798722] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver Micrel KSZ9031 Gigabit PHY
[ 1.809109] cpsw 48484000.ethernet: Detected MACID = a0:f6:fd:bd:76:7c
[ 1.816384] cpsw 48484000.ethernet: cpsw: Detected MACID = a0:f6:fd:bd:76:7d
[ 1.824942] mousedev: PS/2 mouse device common for all mice
[ 1.831038] i2c /dev entries driver
[ 1.836108] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_fan[0]' - status (0)
[ 1.837340] gpio-fan gpio_fan: GPIO fan initialized
[ 1.843275] tmp102 0-0048: initialized
[ 1.850080] omap_hsmmc 4809c000.mmc: GPIO lookup for consumer cd
[ 1.850091] omap_hsmmc 4809c000.mmc: using device tree for GPIO lookup
[ 1.850121] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@4809c000[0]' - status (0)
[ 1.850157] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.854799] omap_hsmmc 4809c000.mmc: GPIO lookup for consumer wp
[ 1.854808] omap_hsmmc 4809c000.mmc: using device tree for GPIO lookup
[ 1.854817] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@4809c000[0]'
[ 1.854826] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@4809c000[0]'
[ 1.854834] omap_hsmmc 4809c000.mmc: using lookup tables for GPIO lookup
[ 1.854842] omap_hsmmc 4809c000.mmc: lookup for GPIO wp failed
[ 1.855172] vdd_3v3: supplied by regen1
[ 1.908509] omap_hsmmc 480b4000.mmc: GPIO lookup for consumer cd
[ 1.908520] omap_hsmmc 480b4000.mmc: using device tree for GPIO lookup
[ 1.908530] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 1.908539] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 1.908548] omap_hsmmc 480b4000.mmc: using lookup tables for GPIO lookup
[ 1.908556] omap_hsmmc 480b4000.mmc: lookup for GPIO cd failed
[ 1.908566] omap_hsmmc 480b4000.mmc: GPIO lookup for consumer wp
[ 1.908573] omap_hsmmc 480b4000.mmc: using device tree for GPIO lookup
[ 1.908581] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480b4000[0]'
[ 1.908590] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480b4000[0]'
[ 1.908598] omap_hsmmc 480b4000.mmc: using lookup tables for GPIO lookup
[ 1.908605] omap_hsmmc 480b4000.mmc: lookup for GPIO wp failed
[ 1.908770] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 1.915154] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 1.978564] omap_hsmmc 480ad000.mmc: GPIO lookup for consumer cd
[ 1.978574] omap_hsmmc 480ad000.mmc: using device tree for GPIO lookup
[ 1.978584] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@480ad000[0]'
[ 1.978593] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@480ad000[0]'
[ 1.978601] omap_hsmmc 480ad000.mmc: using lookup tables for GPIO lookup
[ 1.978609] omap_hsmmc 480ad000.mmc: lookup for GPIO cd failed
[ 1.978619] omap_hsmmc 480ad000.mmc: GPIO lookup for consumer wp
[ 1.978626] omap_hsmmc 480ad000.mmc: using device tree for GPIO lookup
[ 1.978634] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@480ad000[0]'
[ 1.978643] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@480ad000[0]'
[ 1.978650] omap_hsmmc 480ad000.mmc: using lookup tables for GPIO lookup
[ 1.978657] omap_hsmmc 480ad000.mmc: lookup for GPIO wp failed
[ 2.018755] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@0[0]' - status (0)
[ 2.018881] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@1[0]' - status (0)
[ 2.018995] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@2[0]' - status (0)
[ 2.019127] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@3[0]' - status (0)
[ 2.019639] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.030764] NET: Registered protocol family 10
[ 2.046074] sit: IPv6 over IPv4 tunneling driver
[ 2.051373] NET: Registered protocol family 17
[ 2.056059] Key type dns_resolver registered
[ 2.060464] omap_voltage_late_init: Voltage driver support not added
[ 2.067344] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.073568] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.080268] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.086478] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.094641] Power Management for TI OMAP4+ devices.
[ 2.099758] Registering SWP/SWPB emulation handler
[ 2.106607] dmm 4e000000.dmm: initialized all PAT entries
[ 2.131051] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.137694] [drm] No driver support for vblank timestamp query.
[ 2.145965] mmc0: host does not support reading read-only switch, assuming write-enable
[ 2.156696] mmc0: new high speed SDHC card at address 0007
[ 2.172569] mmcblk0: mmc0:0007 SD08G 7.42 GiB
[ 2.178393] mmcblk0: p1 p2
[ 2.222855] mmc1: MAN_BKOPS_EN bit is not set
[ 2.235805] mmc1: new DDR MMC card at address 0001
[ 2.240927] mmcblk1: mmc1:0001 S10004 3.56 GiB
[ 2.245619] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
[ 2.251722] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
[ 2.258233] mmcblk1: p1 p2 p3
[ 2.412129] [drm] Enabling DMM ywrap scrolling
[ 2.451052] Console: switching to colour frame buffer device 100x30
[ 2.459937] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.488554] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.495124] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_keys/USER1[0]' - status (0)
[ 2.495155] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_keys/USER2[0]' - status (0)
[ 2.495184] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_keys/USER3[0]' - status (0)
[ 2.495211] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_keys/USER4[0]' - status (0)
[ 2.495237] of_get_named_gpiod_flags: parsed 'gpios' property of node '/gpio_keys/USER5[0]' - status (0)
[ 2.495858] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[ 2.502823] hctosys: unable to open rtc device (rtc0)
[ 2.518100] net eth0: initializing cpsw version 1.15 (0)
[ 2.523491] net eth0: initialized cpsw ale version 1.4
[ 2.528666] net eth0: ALE Table size 1024
[ 2.620640] net eth0: phy found : id is : 0x221622
[ 2.631976] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 2.637861] net eth1: initializing cpsw version 1.15 (0)
[ 2.730359] net eth1: phy found : id is : 0x221622
[ 2.740126] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 6.626911] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 6.638305] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 6.658289] Sending DHCP requests ., OK
[ 6.718293] IP-Config: Got DHCP answer from 192.168.3.254, my address is 192.168.3.204
[ 6.739213] IP-Config: Complete:
[ 6.742460] device=eth0, hwaddr=a0:f6:fd:bd:76:7c, ipaddr=192.168.3.204, mask=255.255.255.0, gw=192.168.3.254
[ 6.752872] host=192.168.3.204, domain=, nis-domain=(none)
[ 6.758834] bootserver=0.0.0.0, rootserver=192.168.3.221, rootpath=
[ 6.765387] nameserver0=192.168.3.254
[ 6.769860] aic_dvdd_fixed: disabling
[ 6.773538] vmmcwl_fixed: disabling
[ 6.777211] ldousb: disabling
[ 6.780711] ALSA device list:
[ 6.783691] No soundcards found.
[ 6.811526] VFS: Mounted root (nfs filesystem) on device 0:15.
[ 6.818203] devtmpfs: mounted
[ 6.821405] Freeing unused kernel memory: 332K (c08c1000 - c0914000)
[ 6.827786] This architecture does not have kernel memory protection.
[ 6.972992] systemd[1]: System time before build time, advancing clock.
[ 7.004063] random: systemd: uninitialized urandom read (16 bytes read, 67 bits of entropy available)
[ 7.019226] random: systemd: uninitialized urandom read (16 bytes read, 69 bits of entropy available)
[ 7.030659] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 7.049138] systemd[1]: Detected architecture arm.
[ 7.070313] systemd[1]: Set hostname to <am57xx-evm>.
[ 7.154465] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 80 bits of entropy available)
[ 7.178467] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 83 bits of entropy available)
[ 7.222201] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 86 bits of entropy available)
[ 7.313090] random: systemd: uninitialized urandom read (16 bytes read, 93 bits of entropy available)
[ 7.322583] random: systemd: uninitialized urandom read (16 bytes read, 93 bits of entropy available)
[ 7.341597] random: systemd: uninitialized urandom read (16 bytes read, 94 bits of entropy available)
[ 7.351777] random: systemd: uninitialized urandom read (16 bytes read, 94 bits of entropy available)
[ 7.383629] random: systemd: uninitialized urandom read (16 bytes read, 98 bits of entropy available)
[ 7.625119] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 7.640552] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 7.648248] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 7.655533] systemd[1]: sysinit.target: Found dependency on sockets.target/start
[ 7.662975] systemd[1]: sysinit.target: Found dependency on avahi-daemon.socket/start
[ 7.670855] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 7.678298] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 7.687755] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[ 7.721590] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 7.749718] systemd[1]: Listening on Network Service Netlink Socket.
[ 7.784421] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 7.819238] systemd[1]: Listening on udev Kernel Socket.
[ 7.840077] systemd[1]: Created slice System Slice.
[ 7.859056] systemd[1]: Created slice User and Session Slice.
[ 7.878454] systemd[1]: Reached target Slices.
[ 7.899070] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 7.920564] systemd[1]: Listening on Journal Socket (/dev/log).
[ 7.938628] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 7.968449] systemd[1]: Reached target Paths.
[ 7.988458] systemd[1]: Reached target Swap.
[ 8.009667] systemd[1]: Listening on Journal Socket.
[ 8.058654] systemd[1]: Starting Setup Virtual Console...
[ 8.081504] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 8.086134] random: nonblocking pool is initialized
[ 8.122838] systemd[1]: Mounting Temporary Directory...
[ 8.188677] systemd[1]: Starting Create list of required static device nodes for the current kernel...
[ 8.220666] systemd[1]: Mounting Debug File System...
[ 8.234899] systemd[1]: Mounting POSIX Message Queue File System...
[ 8.258643] systemd[1]: Reached target Remote File Systems.
[ 8.289257] systemd[1]: Created slice system-getty.slice.
[ 8.319243] systemd[1]: Listening on Syslog Socket.
[ 8.388699] systemd[1]: Starting Journal Service...
[ 8.425925] systemd[1]: Starting Load Kernel Modules...
[ 8.437813] systemd[1]: Listening on udev Control Socket.
[ 8.466272] CMEMK module: reference Linux version 4.4.19
[ 8.481385] allocated heap buffer 0x40500000 of size 0x100000
[ 8.487186] cmemk initialized
[ 8.507464] cryptodev: driver 1.8 loaded.
[ 8.515637] systemd[1]: Mounted POSIX Message Queue File System.
[ 8.548673] systemd[1]: Mounted Debug File System.
[ 8.568588] systemd[1]: Mounted Temporary Directory.
[ 8.588756] systemd[1]: Started Journal Service.
[ 9.199318] systemd-journald[143]: Received request to flush runtime journal from PID 1
[ 9.628236] omap-rproc 58820000.ipu: assigned reserved memory node ipu1_cma@9d000000
[ 9.673321] remoteproc0: 58820000.ipu is available
[ 9.684910] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 9.720834] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 9.737838] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
[ 9.750770] remoteproc1: 55020000.ipu is available
[ 9.760352] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 9.781686] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 9.794189] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
[ 9.807731] remoteproc2: 40800000.dsp is available
[ 9.826558] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 9.841370] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 9.855940] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[ 9.864821] remoteproc3: 41000000.dsp is available
[ 9.870336] remoteproc3: Note: remoteproc is still under development and considered experimental.
[ 9.880073] remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.184998] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 10.236766] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp/i2c@48070000/tlv320aic3104@18[0]'
[ 10.237618] aic_dvdd_fixed: supplied by vdd_3v3
[ 10.248621] rtc-ds1307 2-006f: read: 81 10 21 2a 03 30 16
[ 10.248639] rtc-ds1307 2-006f: read secs=1, mins=10, hours=21, mday=3, mon=9, year=116, wday=1
[ 10.251248] rtc-ds1307 2-006f: read: 81 10 21 2a 03 30 16
[ 10.251259] rtc-ds1307 2-006f: read secs=1, mins=10, hours=21, mday=3, mon=9, year=116, wday=1
[ 10.251835] alg: skcipher: setkey failed on test 5 for ecb-des-omap: flags=100
[ 10.251987] rtc-ds1307 2-006f: mcp794xx_read_alarm, sec=0 min=0 hour=0 wday=0 mday=1 mon=0 enabled=0 polarity=0 irq=0 match=0
[ 10.261133] rtc-ds1307 2-006f: read: 81 10 21 2a 03 30 16
[ 10.261145] rtc-ds1307 2-006f: read secs=1, mins=10, hours=21, mday=3, mon=9, year=116, wday=1
[ 10.261153] rtc rtc0: alarm rollover: year
[ 10.262137] rtc-ds1307 2-006f: read: 81 10 21 2a 03 30 16
[ 10.262148] rtc-ds1307 2-006f: read secs=1, mins=10, hours=21, mday=3, mon=9, year=116, wday=1
[ 10.262993] rtc rtc0: mcp7941x: dev (254:0)
[ 10.263010] rtc-ds1307 2-006f: rtc core: registered mcp7941x as rtc0
[ 10.269937] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
[ 10.284505] rtc-ds1307 2-006f: got IRQ 471
[ 10.284530] rtc-ds1307 2-006f: 64 bytes nvram
[ 10.285478] adv7842 4-0020: detecting adv7842 client on address 0x40
[ 10.325575] alg: skcipher-ddst: setkey failed on test 5 for ecb-des-omap: flags=100
[ 10.351212] adv7842 4-0020: adv7842_s_detect_tx_5v_ctrl: 0x0 -> 0x0
[ 10.369140] rtc rtc1: 48070000.i2c:tps659: dev (254:1)
[ 10.369156] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659 as rtc1
[ 10.408246] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 10.442954] adv7842 4-0020: set_rgb_quantization_range: RGB quantization range: 0, RGB out: 0, HDMI: 0
[ 10.442966] adv7842 4-0020: adv7842_set_gain: Auto gain: a = 0x100, b = 0x100, c = 0x100
[ 10.443146] adv7842 4-0020: adv7842_set_offset: Auto offset: a = 0x3ff, b = 0x3ff, c = 0x3ff
[ 10.443729] adv7842 4-0020: adv7842_set_gain: Manual gain: a = 0xe0, b = 0xe0, c = 0xe0
[ 10.443916] adv7842 4-0020: adv7842_set_offset: Manual offset: a = 0x70, b = 0x70, c = 0x70
[ 10.457254] adv7842 4-0020: R 0, G 0, B 0
[ 10.457272] adv7842 4-0020: Y 10, U 80, V 80
[ 10.466190] adv7842 4-0020: set_rgb_quantization_range: RGB quantization range: 0, RGB out: 0, HDMI: 0
[ 10.466298] adv7842 4-0020: adv7842_set_gain: Auto gain: a = 0x100, b = 0x100, c = 0x100
[ 10.469884] adv7842 4-0020: adv7842_set_offset: Auto offset: a = 0x3ff, b = 0x3ff, c = 0x3ff
[ 10.475651] adv7842 4-0020: adv7842_set_gain: Manual gain: a = 0xe0, b = 0xe0, c = 0xe0
[ 10.475878] adv7842 4-0020: adv7842_set_offset: Manual offset: a = 0x70, b = 0x70, c = 0x70
[ 10.477617] adv7842 4-0020: adv7842 found @ 0x40 (OMAP I2C adapter)
[ 10.492231] pixcir_ts 4-005c: GPIO lookup for consumer attb
[ 10.492247] pixcir_ts 4-005c: using device tree for GPIO lookup
[ 10.492259] of_get_named_gpiod_flags: can't parse 'attb-gpios' property of node '/ocp/i2c@4807c000/pixcir_ts@5c[0]'
[ 10.492285] of_get_named_gpiod_flags: parsed 'attb-gpio' property of node '/ocp/i2c@4807c000/pixcir_ts@5c[0]' - status (0)
[ 10.492299] pixcir_ts 4-005c: GPIO lookup for consumer reset
[ 10.492306] pixcir_ts 4-005c: using device tree for GPIO lookup
[ 10.492314] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/i2c@4807c000/pixcir_ts@5c[0]'
[ 10.492334] of_get_named_gpiod_flags: parsed 'reset-gpio' property of node '/ocp/i2c@4807c000/pixcir_ts@5c[0]' - status (0)
[ 10.496269] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: GPIO lookup for consumer id
[ 10.496293] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using device tree for GPIO lookup
[ 10.496308] of_get_named_gpiod_flags: can't parse 'id-gpios' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 10.496317] of_get_named_gpiod_flags: can't parse 'id-gpio' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 10.496324] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using lookup tables for GPIO lookup
[ 10.496332] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: lookup for GPIO id failed
[ 10.496339] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: GPIO lookup for consumer vbus
[ 10.496344] palmas-usb 48070000.i2c:tps659038@58:tps659038_usb: using device tree for GPIO lookup
[ 10.496351] of_get_named_gpiod_flags: can't parse 'vbus-gpios' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]'
[ 10.496398] of_get_named_gpiod_flags: parsed 'vbus-gpio' property of node '/ocp/i2c@48070000/tps659038@58/tps659038_usb[0]' - status (0)
[ 10.529839] remoteproc1: registered virtio0 (type 7)
[ 10.600786] input: pixcir_tangoc as /devices/platform/44000000.ocp/4807c000.i2c/i2c-4/4-005c/input/input1
[ 10.677307] remoteproc0: registered virtio1 (type 7)
[ 10.735014] rtc rtc2: 48838000.rtc: dev (254:2)
[ 10.735028] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc2
[ 10.920735] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 10.949477] vpe 489d0000.vpe: Device registered as /dev/video0
[ 11.136300] SCSI subsystem initialized
[ 11.161266] vip2-s0: vip_set_slice_path:
[ 11.161279] vip2-s0: vip_set_slice_path: DATA_PATH_SELECT(0000010C): 80008000
[ 11.162391] vip2-s1: vip_set_slice_path:
[ 11.162404] vip2-s1: vip_set_slice_path: DATA_PATH_SELECT(00000110): 80008000
[ 11.162433] vip 48990000.vip: loading firmware vpdma-1b8.bin
[ 11.188419] vip 48990000.vip: VPDMA firmware loaded
[ 11.197523] vip2-s0: can't get next endpoint: loop: 1
[ 11.197534] vip2-s0: register async notifier for 1 subdevs
[ 11.197542] vip2-s0: vip_async_bound
[ 11.197548] vip2-s0: Port A: Using subdev adv7842 4-0020 for capture
[ 11.209068] vip2-s0: subdev adv7842 4-0020: code: 100a idx: 0
[ 11.209079] vip2-s0: matched fourcc: RGB3: code: 100a idx: 0
[ 11.209086] vip2-s0: subdev adv7842 4-0020: code: 2008 idx: 1
[ 11.209092] vip2-s0: subdev adv7842 4-0020: code: 2009 idx: 2
[ 11.209097] vip2-s0: subdev adv7842 4-0020: code: 200b idx: 3
[ 11.209102] vip2-s0: subdev adv7842 4-0020: code: 200c idx: 4
[ 11.209107] vip2-s0: subdev adv7842 4-0020: code: 201e idx: 5
[ 11.209112] vip2-s0: subdev adv7842 4-0020: code: 201f idx: 6
[ 11.209116] vip2-s0: subdev adv7842 4-0020: code: 200f idx: 7
[ 11.209120] vip2-s0: subdev adv7842 4-0020: code: 2010 idx: 8
[ 11.209125] vip2-s0: subdev adv7842 4-0020: code: 2011 idx: 9
[ 11.209129] vip2-s0: subdev adv7842 4-0020: code: 2012 idx: 10
[ 11.209134] vip2-s0: subdev adv7842 4-0020: code: 201a idx: 11
[ 11.209138] vip2-s0: subdev adv7842 4-0020: code: 201b idx: 12
[ 11.209143] vip2-s0: subdev adv7842 4-0020: code: 200d idx: 13
[ 11.209148] vip2-s0: subdev adv7842 4-0020: code: 200e idx: 14
[ 11.209152] vip2-s0: subdev adv7842 4-0020: code: 2020 idx: 15
[ 11.209157] vip2-s0: subdev adv7842 4-0020: code: 2021 idx: 16
[ 11.209161] vip2-s0: subdev adv7842 4-0020: code: 2022 idx: 17
[ 11.209165] vip2-s0: subdev adv7842 4-0020: code: 2023 idx: 18
[ 11.209183] vip2-s0: vip_async_complete
[ 11.231875] libata version 3.00 loaded.
[ 11.304869] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 11.333138] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 11.342869] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 11.379804] scsi host0: ahci
[ 11.387811] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 348
[ 11.463457] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 11.478627] ti-pruss 4b200000.pruss: creating PRU cores and other child platform devices
[ 11.489903] irq: no irq domain found for /ocp/pruss@4b200000/intc@4b220000 !
[ 11.500457] irq: no irq domain found for /ocp/pruss@4b200000/intc@4b220000 !
[ 11.512768] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 11.796734] rtc-ds1307 2-006f: write secs=15, mins=6, hours=21, mday=3, mon=9, year=116, wday=1
[ 11.796799] rtc-ds1307 2-006f: write: 95 06 21 0a 03 10 16
[ 11.804208] rtc-ds1307 2-006f: read: 95 06 21 2a 03 30 16
[ 11.804222] rtc-ds1307 2-006f: read secs=15, mins=6, hours=21, mday=3, mon=9, year=116, wday=1
[ 11.808630] ata1: SATA link down (SStatus 0 SControl 300)
[ 12.123693] remoteproc3: registered virtio2 (type 7)
[ 12.144573] remoteproc2: registered virtio3 (type 7)
[ 12.233819] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
[ 12.269707] FAT-fs (mmcblk1p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.284564] EXT4-fs (mmcblk0p2): mounting ext3 file system using the ext4 subsystem
[ 12.297466] FAT-fs (mmcblk1p2): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.335548] FAT-fs (mmcblk1p3): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.383724] ti-pruss 4b280000.pruss: creating PRU cores and other child platform devices
[ 12.393135] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 12.411120] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 12.434337] irq: no irq domain found for /ocp/pruss@4b280000/intc@4b2a0000 !
[ 12.447124] irq: no irq domain found for /ocp/pruss@4b280000/intc@4b2a0000 !
[ 12.457979] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 12.478116] remoteproc4: 4b234000.pru0 is available
[ 12.488231] remoteproc4: Note: remoteproc is still under development and considered experimental.
[ 12.507942] remoteproc4: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.554763] remoteproc4: registered virtio4 (type 7)
[ 12.565348] pru-rproc 4b234000.pru0: PRU rproc node /ocp/pruss@4b200000/pru0@4b234000 probed successfully
[ 12.587160] remoteproc5: 4b238000.pru1 is available
[ 12.592437] remoteproc5: Note: remoteproc is still under development and considered experimental.
[ 12.622940] remoteproc5: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.661555] remoteproc5: registered virtio5 (type 7)
[ 12.676521] pru-rproc 4b238000.pru1: PRU rproc node /ocp/pruss@4b200000/pru1@4b238000 probed successfully
[ 12.724928] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 12.729293] remoteproc6: 4b2b4000.pru0 is available
[ 12.729296] remoteproc6: Note: remoteproc is still under development and considered experimental.
[ 12.729299] remoteproc6: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.762824] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
[ 12.794491] remoteproc6: registered virtio6 (type 7)
[ 12.800687] pru-rproc 4b2b4000.pru0: PRU rproc node /ocp/pruss@4b280000/pru0@4b2b4000 probed successfully
[ 12.827651] remoteproc7: 4b2b8000.pru1 is available
[ 12.833462] remoteproc7: Note: remoteproc is still under development and considered experimental.
[ 12.859149] remoteproc7: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.896086] remoteproc7: registered virtio7 (type 7)
[ 12.902574] pru-rproc 4b2b8000.pru1: PRU rproc node /ocp/pruss@4b280000/pru1@4b2b8000 probed successfully
[ 13.018027] of_get_named_gpiod_flags: can't parse 'simple-audio-card,hp-det-gpio' property of node '/sound@0[0]'
[ 13.018039] of_get_named_gpiod_flags: can't parse 'simple-audio-card,mic-det-gpio' property of node '/sound@0[0]'
[ 13.021627] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 13.572792] Bluetooth: Core ver 2.21
[ 13.595781] NET: Registered protocol family 31
[ 13.648794] Bluetooth: HCI device and connection manager initialized
[ 13.679704] NET: Registered protocol family 15
[ 13.703872] Bluetooth: HCI socket layer initialized
[ 13.741657] Bluetooth: L2CAP socket layer initialized
[ 13.774874] Bluetooth: SCO socket layer initialized
[ 13.958545] Initializing XFRM netlink socket
[ 14.405572] remoteproc1: powering up 55020000.ipu
[ 14.477910] remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3497308
[ 14.524954] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
[ 14.772665] remoteproc1: remote processor 55020000.ipu is now up
[ 14.806990] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 14.810043] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x65
[ 14.810941] virtio_rpmsg_bus virtio0: creating channel rpmsg-rpc addr 0x66
[ 14.881355] remoteproc0: powering up 58820000.ipu
[ 14.922890] remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 4953116
[ 14.950401] omap-iommu 58882000.mmu: 58882000.mmu: version 2.1
[ 14.988124] remoteproc0: remote processor 58820000.ipu is now up
[ 15.020779] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 15.022444] virtio_rpmsg_bus virtio1: creating channel rpmsg-client-sample addr 0x32
[ 15.022598] virtio_rpmsg_bus virtio1: creating channel rpmsg-client-sample addr 0x33
[ 15.023094] virtio_rpmsg_bus virtio1: creating channel rpmsg-omx addr 0x3c
[ 15.023204] virtio_rpmsg_bus virtio1: creating channel rpmsg-rpc addr 0x65
[ 15.084303] remoteproc3: powering up 41000000.dsp
[ 15.167328] remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 22037092
[ 15.193832] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[ 15.199727] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[ 15.205675] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[ 15.280954] remoteproc3: remote processor 41000000.dsp is now up
[ 15.303561] virtio_rpmsg_bus virtio2: rpmsg host is online
[ 15.303639] virtio_rpmsg_bus virtio2: creating channel rpmsg-proto addr 0x3d
[ 15.330828] remoteproc2: powering up 40800000.dsp
[ 15.353917] usbcore: registered new interface driver usbfs
[ 15.394142] usbcore: registered new interface driver hub
[ 15.409495] usbcore: registered new device driver usb
[ 15.425530] remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 22037092
[ 15.440841] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 15.446735] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
[ 15.452696] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
[ 15.466852] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 15.475677] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 15.496108] remoteproc2: remote processor 40800000.dsp is now up
[ 15.502910] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00010010
[ 15.517416] virtio_rpmsg_bus virtio3: rpmsg host is online
[ 15.517728] virtio_rpmsg_bus virtio3: creating channel rpmsg-proto addr 0x3d
[ 15.531025] xhci-hcd xhci-hcd.1.auto: irq 474, io mem 0x48890000
[ 15.541333] remoteproc4: powering up 4b234000.pru0
[ 15.541790] hub 1-0:1.0: USB hub found
[ 15.550923] hub 1-0:1.0: 1 port detected
[ 15.556517] remoteproc4: Booting fw image am57xx-pru1_0-fw, size 74812
[ 15.567965] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 15.575697] ti-pruss 4b200000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 15.590105] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 15.599458] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 15.607845] remoteproc4: remote processor 4b234000.pru0 is now up
[ 15.616164] virtio_rpmsg_bus virtio4: rpmsg host is online
[ 15.621724] virtio_rpmsg_bus virtio4: creating channel rpmsg-pru addr 0x1e
[ 15.633617] hub 2-0:1.0: USB hub found
[ 15.637683] hub 2-0:1.0: 1 port detected
[ 15.651382] remoteproc5: powering up 4b238000.pru1
[ 15.659934] remoteproc5: Booting fw image am57xx-pru1_1-fw, size 74812
[ 15.666908] ti-pruss 4b200000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 15.682592] remoteproc5: remote processor 4b238000.pru1 is now up
[ 15.691302] virtio_rpmsg_bus virtio5: rpmsg host is online
[ 15.696840] virtio_rpmsg_bus virtio5: creating channel rpmsg-pru addr 0x1f
[ 15.712676] remoteproc6: powering up 4b2b4000.pru0
[ 15.720937] remoteproc6: Booting fw image am57xx-pru2_0-fw, size 74812
[ 15.729137] ti-pruss 4b280000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 15.741640] remoteproc6: remote processor 4b2b4000.pru0 is now up
[ 15.750567] virtio_rpmsg_bus virtio6: rpmsg host is online
[ 15.756103] virtio_rpmsg_bus virtio6: creating channel rpmsg-pru addr 0x20
[ 15.781612] remoteproc7: powering up 4b2b8000.pru1
[ 15.799883] remoteproc7: Booting fw image am57xx-pru2_1-fw, size 74812
[ 15.810681] ti-pruss 4b280000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 15.823829] remoteproc7: remote processor 4b2b8000.pru1 is now up
[ 15.832208] virtio_rpmsg_bus virtio7: rpmsg host is online
[ 15.837746] virtio_rpmsg_bus virtio7: creating channel rpmsg-pru addr 0x21
[ 15.888414] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[ 15.903235] rpmsg_pru rpmsg8: new rpmsg_pru device: /dev/rpmsg_pru30
[ 15.911299] rpmsg_pru rpmsg9: new rpmsg_pru device: /dev/rpmsg_pru31
[ 15.928720] rpmsg_pru rpmsg10: new rpmsg_pru device: /dev/rpmsg_pru32
[ 15.938682] rpmsg_rpc rpmsg0: probing service dce-callback with src 1024 dst 101
[ 15.952923] NET: Registered protocol family 41
[ 15.958038] rpmsg_pru rpmsg11: new rpmsg_pru device: /dev/rpmsg_pru33
[ 15.968724] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[ 15.985887] rpmsg_rpc rpmsg1: probing service rpmsg-dce with src 1025 dst 102
[ 15.986259] rpmsg_rpc rpmsg0: published functions = 4
[ 16.016212] hub 2-1:1.0: USB hub found
[ 16.020500] hub 2-1:1.0: 4 ports detected
[ 16.025627] rpmsg_rpc rpmsg5: probing service rpc_example_2 with src 1024 dst 101
[ 16.025952] rpmsg_rpc rpmsg1: published functions = 9
[ 16.091016] rpmsg_rpc rpmsg5: published functions = 8
[ 16.111682] hub 1-1:1.0: USB hub found
[ 16.115985] hub 1-1:1.0: 4 ports detected
[ 17.350987] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 26.045716] omap_hwmod: mmu1_dsp1: _wait_target_disable failed
[ 26.059742] omap_hwmod: mmu1_dsp2: _wait_target_disable failed
[ 26.073500] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
[ 26.087292] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
As you can see the vip is bound to the adv7842 subdevice. The problem is that no /dev/video1 device is registered. What could be the reason for that? Is it allowed to manually set the platform data as I did it in the probe function?
I really would appreciate your help since I am new to v4l2 an linux in general.
Thanks and have e nice day
Marc