Part Number: OMAP-L138
Hello,
I'm using LIDD interface for L138 chip to drive the display. Currently I have an issue that LCD_HSYNC line is causing some noises so I'm wondering if there is a way to make it always low or high?
Currently the LIDD_CTRL setting for mode (bit [2:0]) is set to 100. When I change it to 011, the display is not working anymore. TRM does have a description of LCD_HSYNC in overall architecture section: "The RASTER_TIMING_0 register fully defines the behavior of this signal". Since I'm using LIDD so I'm not sure if this applies.
Thanks for helping.