Part Number: AM3354
Tool/software: Linux
Hi guys:
i just finished building ti processor sdk 03.02.00.05 for AM3354 with success on a 64bit ubuntu environment.
due to company reasons..i now need to build the processor SDK again with a different cross-compiler on a 32bit debian environment.
the original compiler is linaro 5.3 compiler. (x64)
right now i had to change to arm-none-linux-gnueabi-gcc-4.9.1(x86) from mentor graphics.
so.
when i changed the PATH variable and try to build the sdk. i got an error.
here is my steps:
(apt-install all the needed packages needed as usual.and changed the dpkg-reconfigure option as well.)
cd tisdk/build/
. conf/setenv
export PATH=/home/mgc/embedded/codebench/bin:$PATH
export MGLS_LICENSE_FILE=/home/mgc/license.lic
MACHINE=am335x-evm bitbake arago-core-tisdk-image -c cleanall
and then i got :
ERROR: No valid toolchain in PATH
ERROR: Unable to parse TOOLCHAIN_PATH[:=]
Traceback (most recent call last):
File "TOOLCHAIN_PATH[:=]", line 1, in <module>
File "/media/hdd/yandong/arago/tisdk/sources/bitbake/lib/bb/__init__.py", line 104, in fatal:
mainlogger.critical(''.join(args), extra=kwargs)
> raise BBHandledException()
ExpansionError: Failure expanding variable TOOLCHAIN_PATH[:=], expression was ${@bool(d.getVar('TOOLCHAIN_SYSPATH', d, 1)) and (os.path.exists(d.getVar('TOOLCHAIN_SYSPATH', d, 1)) and os.path.dirname(d.getVar('TOOLCHAIN_SYSPATH', d, 1)) or bb.fatal('No valid toolchain in PATH')) or ''} which triggered exception BBHandledException:
ERROR: Error parsing configuration files
Traceback (most recent call last):
File "/media/hdd/yandong/arago/tisdk/sources/bitbake/lib/bb/cookerdata.py", line 258, in CookerDataBuilder.parseBaseConfiguration():
try:
> self.parseConfigurationFiles(self.prefiles, self.postfiles)
except SyntaxError:
File "/media/hdd/yandong/arago/tisdk/sources/bitbake/lib/bb/cookerdata.py", line 318, in CookerDataBuilder.parseConfigurationFiles(prefiles=[], postfiles=[]):
# Handle any INHERITs and inherit the base class
> bbclasses = ["base"] + (data.getVar('INHERIT', True) or "").split()
for bbclass in bbclasses:
AttributeError: 'NoneType' object has no attribute 'getVar'
my questions are :
1.how to fix this error i've seen?
2.is it possible to change the cross-compiler itself? if i understand correctly...some part of sgx graphic accelerator driver module is pre-built with 5.3 compiler already? in that case does that mean that i simply can't change the compiler if i want to use the SGX graphics feature?
thanks you guys. you are always very helpful.
yandong.