Part Number: AM3352
I would like to use ethernet boot to bring up AM335x based board in production line.
MII lines are connected to a switch which needs pin strapping resistors on some pins and which does not provide MII_RXER signal.
The data sheet gives information about ball reset and ball reset relase state of the MII signals, saying all the lines have pulldown resistors activated at reset.
But after reset boot ROM takes over and reconfigures MII related balls to attach CPSW MII to these balls in order to do ethernet boot.
My concern is about the pin configuration in boot ROM: Does the boot ROM leave the pull down resistors at the MII signals enabled (=only alters pin mux), or are any of the pull down resistors disabled for ethernet boot?
Regards
Thomas