Part Number: AM4376
Other Parts Discussed in Thread: AM4372
I have configured Uboot-2016(UART5 for debug console) for custom board(based on AM4376) using device tree. I have loaded SPL using CCS through JTAG and could see the following message in the minicom.
U-Boot SPL 2016.05-00319-g71499d679f-dirty (Jun 22 2017 - 15:29:21)
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Loaded U-boot using CCS through JTAG after the above log entry, but we didn't get any logs.
Following are the SDK details.
ti-processor-sdk-linux-am437x-evm-03.03.00.04-Linux-x86-Install.bin
u-boot-2016.05+gitAUTOINC+4db46a6bbd-g4db46a6bbd
linux-4.4.41+gitAUTOINC+f9f6f0db2d-gf9f6f0db2d