This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

deinterlace for delay



Hi,

When  I use ISS module to capture PAL video,the video 's sawtooth  very bad.So  I  use dei module of hdvpss ((..\ti_tools\hdvpss_01_00_01_37\packages\ti\psp\examples\common\vps\m2m\m2mDeiScale\)。The video became better.But the dei module will bring me one frame delay as 40ms. We analye the video stream by elcard. we find that the frame0 and frame1 of   dei's video is same(dei.264). So can you tell me it is legal or illegal ?  And why?

My dei module parameter is below:

/* Init application object with selected option */
appObj = &M2mDeiObjs;
appObj->mode = DEI_DRIVER_MODE;
appObj->numCh = DEI_NUM_CHANNELS;
appObj->inMemType = DEI_IN_MEM_TYPE;
appObj->outMemTypeVip = DEI_VIP_OUT_MEM_TYPE;
appObj->numInBuffers = DEI_NUM_IN_BUFFERS;
appObj->numOutBuffers = DEI_NUM_IN_BUFFERS;
appObj->inWidth = vcap_params.width;//DEI_IN_WIDTH;
appObj->inHeight = vcap_params.height / 2;//DEI_IN_HEIGHT;
appObj->inDataFmt = DEI_IN_FMT;
appObj->outWidthDei = DEI_OUT0_WIDTH;
appObj->outHeightDei = DEI_OUT0_HEIGHT;
appObj->outWidthVip = vcap_params.width;
appObj->outHeightVip = vcap_params.height;
appObj->outDataFmtVip = DEI_OUT1_FMT;
appObj->drnEnable = FALSE;
appObj->comprEnable = FALSE;
appObj->drvInst = VPS_M2M_INST_MAIN_DEI_SC3_VIP0;

video_stream.zip