This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: How to add DP83630 Ethernet PHY support to Linux

Other Parts Discussed in Thread: OMAP-L138, DP83630, DP83640

Tool/software: Linux

Hi there,

We have an OMAP-L138 Eval board and using the Linux provided with it. I think the Linux kernel version is 3.3.0. 

we have designed a custom board with the OMAP-L138 SoC and have changed the Ethernet PHY when compare to the Eval LCDK board.

we are using DP83630, and would like to add Linux driver for this so that I can using Ethernet from Linux env.

Could someone please, help us with this.

Thanks.