Tool/software: Starterware
Hi experts,
My board is based AM3352, a SPI flash is used to keep SPL/UBOOT image. I created a CCS project based the starterware to access the SPI flash, I was able to write/read flash for now, but the speed is too slow.
1) I'm using blackhawk, I found the maximum clock TCK of it can be like 10MHz.
2) The size of SPL and UBOOT Is like 500KB。
3) While I need like 50 minutes to write this 500KB data.
4) The speed of AM3352 in my GEL is 500MHz.
5) I don't use Interrupt in my project, as I found I couldn't enable Interrupt, I just read 16bytes each time from file, then write it to SPI interface, wait some times (a counter of 0x01FF to zero), then write another 16 bytes again.
6) I measured the timing, I found CCS will write these 16bytes every 1500ms, this should be the root cause, but I don't know how to reduce it.
Any comments?
Thanks
Chris