This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Interfacing DPRAM to GPMC

Part Number: AM5728


Hi all,

I wanted to interface a DPRAM to AM572x EVM.

But when I check the schematics of AM572x EVM, it is found that, the pins gpmc_ad0 to gpmc_ad15(which are required for external interface) are used as  System Boot Select pins.

Is there any alternative way for interfacing a DPRAM to AM572X EVM.

Also I would like to know, whether there is any other TI Processor EVM, in which GPMC pins are freely available for making interface to external devices in parallel mode, at the same, it should have HDMI output, SD card interface.

(In AM335x EVM also GPMC pins are utilized for other purpose )

Thanks for the help in advance.

Thanks & Regards,

Sajeevan.K