Part Number: TMDSEVM6657
Hello Team,
I have a customer who is using the TMDSEVM6657LS EVM. They want to use the Blackhawk USB560v2 System trace device.
" On the TMDSEVM6657LS eval board there is a XDS200 mezzanine card that has a USB and also has a 60 pin MIPI that mates to the emulator. Can they plug the Blackhawk USB560v2 into that MIPI connecter on the XDS200, or do they need to remove the XDS200 mezzanine card, and mate directly to the TI 60 pin on the EVAL board.
If they connect to the MIPI on the XDS200 are there jumpers they need to change in order to bypass the XDS200 and use the Blackhawk device? "
The users guide from enfineon was not very clear about the LS device. What would be the recommended approach for this ?
Thank you for your time.
Sincerely,
Kishen