Hi,
The SDK contains a kernel 2.6.32 which run correctly on the EVM board. This kernel is patched with certainly Unified-patch-03.00.00.05 included in the SDK
I have some questions :
1)Can I apply your patch with a vanilla kernel ? With a kernel 2.6.32.19, I have got a lot of rej file :
kernel_directory# cat ../Unified-patch-03.00.00.05 | patch -p1
./drivers/mfd/twl-core.c.rej
./drivers/net/davinci_emac.c.rej
./drivers/net/can/sja1000/sja1000.c.rej
./drivers/net/can/bfin_can.c.rej
./drivers/net/can/mscan/mscan.c.rej
./drivers/net/can/mcp251x.c.rej
./drivers/net/can/ti_hecc.c.rej
./drivers/usb/musb/Kconfig.rej
./drivers/usb/musb/musb_gadget.c.rej
./drivers/usb/musb/musbhsdma.c.rej
.............;
2)Can I apply your patch with a 2.6.30 kernel ?
I need to apply an adeos patch : adeos-ipipe-2.6.30-arm-1.15-03.patch or adeos-ipipe-2.6.31-arm-1.16-01.patch or adeos-ipipe-2.6.33-arm-1.16-01.patch .
Adeos patch must be applied with a vanilla kernel (without patch). So I would like try to apply adeos patch before OMAP patch.
Regards,