Part Number: AM3352
Champs
On the AM335 GPMC i notice in the TRM it only shows 16 bit address for the synch mode figure 7-23. It does not show the 32 bit address which should be MSB address then LSB address?
1) The question is in the synch AAD mode on the GPMC does it only supports 16 bit address only?
2) if 1 is true then which address is going out on the AD(16:1) the LSB or the MSB?
3) i assume that the other high address lines are not valid in this mode.
Do you have a register setup that you can send me to make for the case of GPMC AAD mode and be able to have the 32 bit lines in Synch mode.
Thanks
regards
Mohsen