Other Parts Discussed in Thread: OMAPL138
Tool/software: Linux
Dear all,
I am confused about the cross compile issue on the OMAPL138 platform.
I am looking for a reference point to cross compile a RTL8192cu Realtek (Edimax) usb wifi adapter for the OMAP.
Does anybody have a experience with this stuff?
What I also not understand is, the OMAPL138 has the 3.3 Kernel,
according the kernel tree, elixir.free-electrons.com/linux/v3.3/source/drivers/net/wireless
there is a wireless file with all wifi drivers, where for example the usb wifi adapter is also included. (rtlwifi)
Why are these drivers not on the OMAP linux kernel?
Thanks