This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: QSPI boot

Guru 15520 points
Part Number: AM4376


Hi,

I have questions about AM437x QSPI boot.

The size of flash memory which AM437x QSPI supporting is up to 64MByte.
In Technical Reference Manual(spruhl7g)page.223 "5.2.6.7 QSPI",
it said "support only 24-bit addressable EEPROM".

Q1.Is this means that RBL only support upto 16MByte(24-bit address) QSPI flash?

Q2.If this size(16MByte) is not enough for user application, does user need to make
user boot loader(secondary bootloader) to load the rest of boot image from QSPI to RAM(internal & external)?

best regards,
g.f.