Part Number: AM5728
Hello, TI Experts,
Our customer sent us a question about the Max frequency spec. for QSPI.
They found the spec. of QSPI_FCLK Max frequency=128MHz in the datasheet (SPRS953C) "Table 5-9. Maximum Supported Frequency".
But they also found the description of "PER_QSPI_CLK=192MHz" in TRM(SPRUHZ6i) "Table 33-17. ROM Code Default Clock Settings".
Question:
Which is correct for Max frequency for QSPI?
128MHz (Datasheet said)?
or
192MHz (TRM said)?
Best regards,