This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: u-boot splash screen for am335x starter kit and beagle bone black with display 4d cape 43t LCD

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

Hello TI,

I need to know, how to bring up the u-boot splash screen in u-boot 2016.05 revision . Please help me add the splash screen to u-boot. I am using am335x starter kit and beagle bone black with display 4d cape 43t lcd.

  • Hello Govindaraji,

    You can use this post as reference.

    Best regards,
    Kemal

  • Hi Kemal,

    I followed the procedure. It is not working with that LCD driver and with changes in u-boot 2016.05
    and even the changes with u-boot Image not booting the Linux kernel also.
  • Can you try with u-boot-2014.7?
  • Hi Kemal,

    I switched to git u-boot branch ti-u-boot-2014.07. And there is no config files in it for the AM335x Starter Kit u-boot configuration.

  • Try:
    git clone git://git.ti.com/ti-u-boot/ti-u-boot.git
    git checkout v2014.07
  • Hi Kemal,

    I couldn't find the u-boot config file for am335x boards from u-boot git revision v2014.07. I can see configs folder only from v2015.04 git revision.
  • The configs directory was introduced later, there is no configs directory in earlier versions.

  • Hi Kemal,

    U-boot splash Screen is working with u-boot  source code(v2016.05) and with AM335x SK board.

    Starter ware examples/evmskAM335x/raster/ code reused for this demonstration (AM335X_StarterWare_02_00_01_01)

    below line added to the u-boot top level Makefile

    +libs-y += drivers/lcd/

    below lines added to the u-boot top board/ti/am335x/board.c

    +#include <rasterDisplay.h>

    add below line to board_init() function of  board/ti/am335x/board.c

    +#ifndef CONFIG_SPL_BUILD
    +  Lcd_Init();//Initialize
    +#endif

    But  when using this u-boot , kernel boot stops after below message

    [    1.066692] [drm] Initialized drm 1.1.0 20060810
    [    1.074126] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    1.080903] [drm] No driver support for vblank timestamp query.

    Guide me how to solve this problem

    and i also wanted to know the license compatible when i use the starter ware code in u-boot?

    last question is after adding the lcd driver support and splash screen, u-boot image size becomes double(1.2MB). due this u-boot delays to load the kernel? and  Is there any way to reduce the final u-boot binary size?

     

  • Hi Kemal,

    After Adding the raster display code into u-boot, splash screen displays at the u-boot stage but kernel loading stops during drm driver  initialization

    below one is kernel boot log

    Starting kernel ...

    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.4.32-gadde2ca9f8 (gtbldadm@ubuntu-16) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 PREE6
    [    0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    [    0.000000] Machine model: TI AM335x EVM-SK
    [    0.000000] cma: Reserved 48 MiB at 0x8a800000
    [    0.000000] Memory policy: Data cache writeback
    [    0.000000] CPU: All CPU(s) started in SVC mode.
    [    0.000000] AM335X ES1.0 (sgx neon )
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 64960
    [    0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=000d9184-02 rw rootfstype=ext4 rootwait loglevel=7
    [    0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
    [    0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
    [    0.000000] Memory: 200280K/262144K available (6595K kernel code, 316K rwdata, 2412K rodata, 268K init, 265K bss, 12712K reserve)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xd0800000 - 0xff800000   ( 752 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xd0000000   ( 256 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc08d4004   (9009 kB)
    [    0.000000]       .init : 0xc08d5000 - 0xc0918000   ( 268 kB)
    [    0.000000]       .data : 0xc0918000 - 0xc0967370   ( 317 kB)
    [    0.000000]        .bss : 0xc0967370 - 0xc09a9a98   ( 266 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000]  Build-time adjustment of leaf fanout to 32.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
    [    0.000000] OMAP clockevent source: timer2 at 24000000 Hz
    [    0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
    [    0.000040] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
    [    0.000053] OMAP clocksource: timer1 at 24000000 Hz
    [    0.000256] clocksource_probe: no matching clocksources found
    [    0.000459] Console: colour dummy device 80x30
    [    0.000490] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.000498] This ensures that you still see kernel messages. Please
    [    0.000504] update your kernel commandline.
    [    0.000524] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
    [    0.118977] pid_max: default: 32768 minimum: 301
    [    0.119116] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.119129] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
    [    0.119909] Initializing cgroup subsys io
    [    0.119944] Initializing cgroup subsys memory
    [    0.119985] Initializing cgroup subsys devices
    [    0.120003] Initializing cgroup subsys freezer
    [    0.120018] Initializing cgroup subsys perf_event
    [    0.120032] Initializing cgroup subsys pids
    [    0.120062] CPU: Testing write buffer coherency: ok
    [    0.120513] Setting up static identity map for 0x80008200 - 0x80008258
    [    0.122942] devtmpfs: initialized
    [    0.137208] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
    [    0.153437] omap_hwmod: debugss: _wait_target_disable failed
    [    0.209383] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.213758] pinctrl core: initialized pinctrl subsystem
    [    0.215220] NET: Registered protocol family 16
    [    0.217659] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.238981] cpuidle: using governor ladder
    [    0.268966] cpuidle: using governor menu
    [    0.274029] OMAP GPIO hardware version 0.1
    [    0.285929] hw-breakpoint: debug architecture 0x4 unsupported.
    [    0.328277] edma 49000000.edma: TI EDMA DMA engine driver
    [    0.329509] reg-fixed-voltage fixedregulator@2: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinme
    [    0.333420] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins,e
    [    0.333599] media: Linux media interface: v0.10
    [    0.333677] Linux video capture interface: v2.00
    [    0.333731] pps_core: LinuxPPS API ver. 1 registered
    [    0.333739] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.333770] PTP clock support registered
    [    0.333829] EDAC MC: Ver: 3.0.0
    [    0.335128] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
    [    0.335542] Advanced Linux Sound Architecture Driver Initialized.
    [    0.336903] clocksource: Switched to clocksource timer1
    [    0.349134] NET: Registered protocol family 2
    [    0.350013] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.350054] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.350085] TCP: Hash tables configured (established 2048 bind 2048)
    [    0.350170] UDP hash table entries: 256 (order: 0, 4096 bytes)
    [    0.350193] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    [    0.350355] NET: Registered protocol family 1
    [    0.350811] RPC: Registered named UNIX socket transport module.
    [    0.350830] RPC: Registered udp transport module.
    [    0.350837] RPC: Registered tcp transport module.
    [    0.350845] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.351900] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
    [    0.354142] futex hash table entries: 256 (order: -1, 3072 bytes)
    [    0.363212] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.364277] NFS: Registering the id_resolver key type
    [    0.364355] Key type id_resolver registered
    [    0.364364] Key type id_legacy registered
    [    0.364459] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.368721] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
    [    0.368755] io scheduler noop registered
    [    0.368769] io scheduler deadline registered
    [    0.368958] io scheduler cfq registered (default)
    [    0.370531] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
    [    0.374035] backlight supply power not found, using dummy regulator
    [    0.443002] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.447684] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
    [    1.063065] console [ttyS0] enabled
    [    1.067874] [drm] Initialized drm 1.1.0 20060810
    [    1.075249] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    1.082037] [drm] No driver support for vblank timestamp query.
    \ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd\ufffd

    Please help to resolve this issue and also give some idea from previous comment questions

  • Hi Kemal,

    I created tilcdc as kernel module and from the module insertion i am getting below logs and am335xevmsk lcd turns to black

    root@am335x-evm:~# dmesg| grep drm
    [ 1.067249] [drm] Initialized drm 1.1.0 20060810
    [ 107.132947] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [ 107.171345] [drm] No driver support for vblank timestamp query.
    [ 107.267348] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
    root@am335x-evm:~# dmesg| grep tilcdc
    [ 107.224320] tilcdc 4830e000.lcdc: fb0: frame buffer device
    [ 107.267348] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
    [ 107.275927] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 107.317803] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.359559] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.401309] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.443053] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.484790] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.526528] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.568265] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.610001] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.651769] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 107.831155] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost flood detected, disabling the interrupt

    Please give me some idea to up the tilcdc driver when rasterDisplay integrated to the u-boot.
  • Please, check this link for some possible causes, likewise display timing, size or other configuration parameters may cause such lost sync.

  • Hi Kemal,

    In that link, Add the Linux kernel configuration “CONFIG_FB_PRE_INIT_FB” to reuse the framebuffer contents that was set up by the U-Boot. but that option not able to enable it in TISDK Linux kernel version 4.4.32.
    Even we tried with changing display timing parameters in u-boot( with rasterDisplay), But still the errors occurred while insmod tilcdc driver in Linux kernel.

    After insmod of tilcdc module the tty service(minicom) gets inactive. above dmesg are taken from ssh

    Please help us solve the issues

    I tried this lists.freedesktop.org/.../104415.html patch to recover the sync lost error in Linux kernel version 4.4.32. But no improvement.
  • The rootfs on your board might be wiped. Can you reflash the SD card and retry?

  • I tried re flashing also, but still the sync lost error occurs when inserting module tilcdc when i use the raster display integrated u-boot

  • Does the board successfully boot until login prompt? Can you switch to the latest U-Boot?

  • yes the board boots successful, but the tty service(minicom) gets inactive while inserting tilcdc driver. tried with u-boot version 2016.05, 2017.01.
    sync lost log i taken it from board ssh.
  • I will be looking at this today.

    Steve K.

  • Hello Steve,

    Any update, regarding Sync lost error in Linux kernel (4.4.32) when using the AM335X_StarterWare_02_00_01_01 raster display code in u-boot (2016.05) for a splash screen.
  • I don't get any Sync lost errors if the generated image.h match the display timings in rasterDisplay.c

    /* Configuring horizontal timing parameter */
    RasterHparamConfig(SOC_LCDC_0_REGS, 480, 4, 8, 43);
    
    /* Configuring vertical timing parameters */
    RasterVparamConfig(SOC_LCDC_0_REGS, 272, 10, 4, 12);
  • i am using same configuration for display timing,  I used below lines to generate the image.h file and i am getting  sync lost error.

    bmpToRaster 480 272 image.bmp ./image.h 24 RGB

    but this image.h file how to match with the rasterDisplay.c display timings .

  • Can you check on your Starter Kit,  whether you will get these errors with the attached u-boot.img?

    md5sum 05c29956a10c721a9b634f8e8a18933d
    sha256sum c4a35c860ba72e0afa4bd9f6ea9cc13bf3bd109ed5a153f2c308649826309642

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/354/3122.u_2D00_boot.img

  • Yes i am getting Sync lost error with my Starter Kit. but getty service working fine as it is

    root@am335x-evm:~# dmesg| grep drm
    [ 1.066737] [drm] Initialized drm 1.1.0 20060810
    [ 1.074184] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [ 1.080971] [drm] No driver support for vblank timestamp query.
    [ 1.207052] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
    [ 12.471974] [drm] Initialized pvr 1.14.3699939 20110701 on minor 1
    root@am335x-evm:~# dmesg| grep tilcdc
    [ 1.096605] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.112751] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.112999] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.114301] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.130995] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 1.137756] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.150733] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 1.170954] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
    [ 1.177734] tilcdc 4830e000.lcdc: fb0: frame buffer device
    [ 1.183606] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.190361] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
    [ 1.207052] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
    [ 1.538141] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost flood detected, disabling the interrupt
    root@am335x-evm:~#
  • The rootfs of which Processor SDK version you are using?

  • ti-processor-sdk-linux-am335x-evm-03.02.00.05
  • 2273.splash.tar.gzCan you use the framebuffer driver already in u-boot. It is in drivers/am335x-fb.c. I've been tasked with coming up with splash screen code and I have it working on the AM335x StarterKit on either 3.2 or 3.3 SDK. I have attached the patches. The LCD data is hard coded for Starter Kit. Currently I'm updating the code to SDK 4.0 and are starting to use the LCD data from the dtb. The image is a gzipped bmp file that is RGB565 and is the size of the screen.

    Steve K.

  • Hi Steve,

    Thank you for your support,

    Starter kit shows splash logo on LCD with the patch and tilcdc sync lost not occurred

    Since am335x_evm_splash_defconfig gives the compilation error with the patch i did one below changes in configs/am335x_evm_defconfig

    +CONFIG_SYS_EXTRA_OPTIONS="NAND,SPLASH"

    but blue and red colors are interchanged.
    to resolve the this we should use below line in dts file
    blue-and-red-wiring = "crossed";

    To use the custom lcd with the beagle bone black please guide me, to change the values of display timing and panel-info.

    and i am not clear on below dts parameter in board.c

    + pnltmp.pxl_clk_div = 2;

    + pnltmp.pup_delay = 1;
    + pnltmp.pon_delay = 1;
    + panel_info.vl_rot = 0;

    + .vl_bpix = 4,
    + .priv = 0


    In future we are planning to use 24 bit image RGB888. is that possible to have 24 bit u-boot splash logo?
  • Hi Steve,

    Please update the u-boot frame-buffer driver patch to use the LCD data from DTB for the u-boot splash screen.
  • Hi Steve,

    with that patch u-boot splash screen logo's Blue and Red colors swapped. how to make, do not swap color with in am335x-fb driver
  • hay bro i try tutorial from u but when i compiled the u-boot show error like this

    ../drivers/lcd/rasterDisplay.c: In function 'Lcd_Init':
    ../drivers/lcd/rasterDisplay.c:21:37: error: 'image1' undeclared (first use in this function)
    (unsigned int)image1,
    ^~~~~~
    ../drivers/lcd/rasterDisplay.c:21:37: note: each undeclared identifier is reported only once for each function it appears in
    ../scripts/Makefile.build:280: recipe for target 'drivers/lcd/rasterDisplay.o' failed
    make[2]: *** [drivers/lcd/rasterDisplay.o] Error 1
    /u-boot/Makefile:1214: recipe for target 'drivers/lcd' failed
    make[1]: *** [drivers/lcd] Error 2
    make[1]: Leaving directory '/u-boot/am335x_evm'
    Makefile:149: recipe for target 'sub-make' failed
    make: *** [sub-make] Error 2

    what must i do? please help :(
  • image1 is output of bmptoraster tool this you should include in your rasterDisplay.c

  • like this?

    /**
    * \file rasterDisplay.c
    *
    * \brief Sample application for raster
    *
    */

    #include "soc_AM335x.h"
    #include "evmskAM335x.h"
    #include "raster.h"
    #include "image.h"



    static void SetUpLCD(void);

    void Lcd_Init(void)
    {
    LCDBackLightEnable();
    SetUpLCD();

    RasterDMAFBConfig(SOC_LCDC_0_REGS,
    (unsigned int)image1,
    (unsigned int)image1 + sizeof(image1) - 2,
    0);

    RasterDMAFBConfig(SOC_LCDC_0_REGS,
    (unsigned int)image1,
    (unsigned int)image1 + sizeof(image1) - 2,
    1);

    RasterEnable(SOC_LCDC_0_REGS);
    }
  • like this?

    /**
    * \file rasterDisplay.c
    *
    * \brief Sample application for raster
    *
    */

    #include "soc_AM335x.h"
    #include "evmskAM335x.h"
    #include "raster.h"
    #include "image.h"

    static void SetUpLCD(void);

    void Lcd_Init(void)
    {
    LCDBackLightEnable();
    SetUpLCD();

    RasterDMAFBConfig(SOC_LCDC_0_REGS,
    (unsigned int)image1,
    (unsigned int)image1 + sizeof(image1) - 2,
    0);

    RasterDMAFBConfig(SOC_LCDC_0_REGS,
    (unsigned int)image1,
    (unsigned int)image1 + sizeof(image1) - 2,
    1);

    RasterEnable(SOC_LCDC_0_REGS);
    }

    i have done that...
  • i have done this tutorial but i get some error like this, could you help me what must i do?


    ../board/ti/am335x/board.c:38:27: fatal error: rasterDisplay.h: No such file or directory
    #include <rasterDisplay.h>
    ^
    compilation terminated.
    ../scripts/Makefile.build:280: recipe for target 'board/ti/am335x/board.o' failed
    make[2]: *** [board/ti/am335x/board.o] Error 1
    /home/daunbiru/ti-processor-sdk-linux-am335x-evm-04.00.00.04/board-support/u-boot-2017.01+gitAUTOINC+9fd60700db-g9fd60700db/Makefile:1233: recipe for target 'board/ti/am335x' failed
    make[1]: *** [board/ti/am335x] Error 2
    make[1]: Leaving directory '/home/daunbiru/ti-processor-sdk-linux-am335x-evm-04.00.00.04/board-support/u-boot-2017.01+gitAUTOINC+9fd60700db-g9fd60700db/am335x_evm'
    Makefile:149: recipe for target 'sub-make' failed
    make: *** [sub-make] Error 2