Part Number: DM388
Hi,
I try to move our source code from ipnc_rdk_3.8 to ipnc_rdk_3.9 for MCFW.
But I found some structs to be changed.
Do you have any document for the new version?
It's still the old version (Document Revision 2.10) in the ipnc_rdk_3.9,
but the Revision History shows it has v2.11.
2.10 20 Jan 2014 Updated for IPNC RDK 3.8 GA release
2.11 9 Dec 2016 Updated for IPNC RDK 3.9 GA release
For example,
V3.9
/**
\brief Mega Pixel Scalar link create parameters
*/
typedef struct MpSclrLink_CreateParams
{
System_LinkInQueParams inQueParams;
/**< Input queue information. */
System_LinkOutQueParams outQueParams;
/**< Output queue information. */
UInt32 pathId;
/**< Instace of scalar to be used */
UInt32 numCh;
/**< Number of channels required */
UInt32 enableLineSkip;
/**< Line skip config */
} MpSclrLink_CreateParams;
V3.8
/**
\brief Mega Pixel Scalar link create parameters
*/
typedef struct MpSclrLink_CreateParams
{
System_LinkInQueParams inQueParams;
/**< Input queue information. */
System_LinkOutQueParams outQueParams;
/**< Output queue information. */
UInt32 pathId;
/**< Instace of scalar to be used */
UInt32 numCh;
/**< Number of channels required */
UInt32 enableLineSkip;
/**< Line skip config */
UInt32 width;
/**< ouput width */
UInt32 height;
/**< ouput height */
} MpSclrLink_CreateParams;
Thanks.
S.K.