This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467 EVM NAND Linux binaries

Hello,

Does anybody have original Linux kernel and ramdisk binaries that are shipped with the SDI DM6467 EVM board? I have accidentaly erased NAND flash, lost Linux, and cannot locate these files on the accompanying DVD disks. It might be that someone has saved the NAND contents in a binary file; this would also work for me. I can store data to flash by either ways, with CCS + NANDWriter or using Flash and Boot utilities (RBL+UBL+APP/U-BOOT). 

I have to restore the EVM to its original state; but I am not a Linux expert, so it would be close to impossible for me to build the kernel and ramdisk from scratch. I serached the DVDs, but there is no ramdisk binary.

Thanks.

Andrew <andrew dot nesterov at techemail dot com>