i am trying to put linux on my custom board DM6446.I am done with the UBL,U-BOOT ,uImage(kernel) and the filesystem.
Have refrred the busybox as my file system.I am using the open source code from git.Here is what i get
## Booting kernel from Legacy Image at 80000000 ...
Image Name: Linux-2.6.31-rc5-davinci1
Image Type: ARM Linux Kernel Image
(uncompressed)
Data Size: 1542436 Bytes = 1.5 MB
Load Address: 80008000
Entry Point:
80008000
Verifying Checksum ... OK
Loading Kernel Image ...
OK
OK
Starting kernel ...
Uncompressing Linux..............................................................
Linux version 2.6.31-rc5-davinci1 (root@localhost.localdomain) (gcc version 4.2.9
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
CPU: VIVT data cache, VIVT instruction
cache
Machine: DaVinci DM644x EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci dm6446a variant
0x1
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 30480
Kernel command line: console=ttyS0,115200n8 root=/dev/ram0 rw initrd=0x81600000,M
PID hash table entries: 512 (order: 9, 2048 bytes)
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table
entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 108116KB available (2856K code, 300K data, 124K init, 0K highmem)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
NR_IRQS:229
Console: colour dummy device 80x30
Calibrating delay loop... 147.86 BogoMIPS (lpj=739328)
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
DaVinci: 71 gpio
irqs
NET: Registered protocol family 16
WARNING: both IDE and Flash are enabled, but they share AEMIF pins.
Disable IDE for NAND/NOR
support.
MUX: Setting register HPIEN_DISABLE
PINMUX0 (0x00000000) = 0x80000c1f -> 0x80000c1f
MUX: initialized
ATAEN
MUX: Setting register ATAEN
PINMUX0 (0x00000000) = 0x80000c1f -> 0x80020c1f
MUX:
initialized HDIREN
MUX: Setting register HDIREN
PINMUX0 (0x00000000) = 0x80020c1f -> 0x80030c1f
MUX:
initialized MCBSP
MUX: Setting register MCBSP
PINMUX1 (0x00000004) = 0x00000081 -> 0x00000481
bio: create slab <bio-0> at 0
pcf857x: probe of 1-0038 failed with error -121
pcf857x: probe of 1-0039 failed with error -121
pcf857x: probe of 1-003a failed with error
-121
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 2, 16384
bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP reno registered
NET: Registered protocol family
1
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory:
10240K
msgmni has been set to 231
io scheduler noop
registered
io scheduler anticipatory registered (default)
Setting Up Clocks for DM420 OSD
Console: switching to colour frame buffer device
90x30
fb0: dm_osd0_fb frame buffer device
fb1: dm_vid0_fb frame buffer device
fb2: dm_osd1_fb frame buffer
device
fb3: dm_vid1_fb frame buffer device
Serial: 8250/16550 driver, 3 ports, IRQ sharing disabled
Platform driver 'serial8250' needs updating - please use dev_pm_ops
serial8250.0: ttyS0
at MMIO 0x1c20000 (irq = 40) is a 16550A
console [ttyS0] enabled
serial8250 serial8250.0: unable to register port at index 1 (IO0 MEM1c20400 IRQ42
serial8250 serial8250.0: unable to register port at index 2 (IO0 MEM1c20800 IRQ42
brd: module
loaded
at24 1-0050: 32768 byte 24c256 EEPROM (writable)
davinci_emac_probe: using random MAC addr: 9a:c3:b8:e1:ad:db
emac-mii:
probed
Fixed MDIO Bus: probed
Platform driver 'smc91x' needs updating - please use dev_pm_ops
Platform driver 'smc911x'
needs updating - please use dev_pm_ops
dm9000 Ethernet Driver, V1.31
Platform driver 'dm9000' needs updating - please use dev_pm_ops
console [netcon0]
enabled
netconsole: network logging started
i2c /dev entries
driver
TCP cubic registered
NET: Registered protocol family
17
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
Clocks: disable unused
uart1
Clocks: disable unused uart2
Clocks: disable unused
ide
Clocks: disable unused asp0
Clocks: disable unused
mmcsd
Clocks: disable unused spi
Clocks: disable unused
usb
Clocks: disable unused vlynq
Clocks: disable unused
pwm0
Clocks: disable unused pwm1
Clocks: disable unused
pwm2
Clocks: disable unused timer1
RAMDISK: ext2 filesystem found at block 0
RAMDISK: Loading
7000KiB [1 disk] into ram disk... done.
VFS: Mounted root (ext2 filesystem) on device 1:0.
Freeing init memory: 124K
System initialization...
Hostname : OMAP3EVM
Filesystem :
v1.0.0
Kernel release : Linux 2.6.31-rc5-davinci1
Kernel version : #1 PREEMPT Mon Oct 5 09:45:44 PKT 2009
Mounting /proc : [SUCCESS]
Mounting /sys :
[SUCCESS]
Mounting /dev : [SUCCESS]
Mounting /dev/pts : [SUCCESS]
Enabling hot-plug : [SUCCESS]
Populating /dev : [SUCCESS]
Mounting other filesystems :
[SUCCESS]
Starting syslogd : [SUCCESS]
Starting telnetd : [SUCCESS]
System initialization complete.
Please press Enter to activate this console.
# ifconfig -a
eth0 Link encap:Ethernet HWaddr 00:00:00:00:00:00
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:4294967295 frame:4294967291
TX packets:0 errors:0 dropped:0 overruns:4294967295 carrier:4294967295
collisions:4294967293
txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:13
lo Link encap:Local Loopback
LOOPBACK MTU:16436
Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0
txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
# ifconfig eth0 up
eth0: no PHY found
ifconfig: SIOCSIFFLAGS: Operation not permitted
# ifconfig eth0 up
net eth0: DaVinci EMAC: request_irq() failed
ifconfig: SIOCSIFFLAGS: Device or resource busy
ifconfig eth0
up
kernel BUG at include/linux/netdevice.h:439!
Unable to handle kernel NULL pointer dereference at virtual address 00000000
pgd =
c1660000
[00000000] *pgd=86668031, *pte=00000000, *ppte=00000000
Internal error: Oops: 817 [#1] PREEMPT
Modules linked
in:
CPU: 0 Not tainted (2.6.31-rc5-davinci1 #1)
PC is at
__bug+0x20/0x2c
LR is at preempt_schedule+0x48/0x64
pc : [<c002b3b0>] lr : [<c024c9e4>] psr: 60000013
sp : c70dbdc0 ip : c70dbd00 fp :
c70dbdcc
r10: c704a800 r9 : c704a800 r8 : c704aac0
r7 : 00000001 r6 : 00000001 r5 : 00000000 r4 : c66dda80
r3 : 00000000 r2 : c70da000 r1 : c706a320 r0 : 00000033
Flags: nZCv IRQs on
FIQs on Mode SVC_32 ISA ARM Segment user
Control: 0005317f Table: 81660000 DAC: 00000015
Process ifconfig (pid: 857, stack limit = 0xc70da270)
Stack: (0xc70dbdc0 to 0xc70dc000)
bdc0: c70dbe1c c70dbdd0
c0191e24 c002b3a0 c704a800 c704a800 c005695c c00568ac
bde0: 00000000 00000000 c704aa08 c704aa08 c0056984 c704a800 c704a830 c0260c8c
be00: 00001002 bee95950 c704a800 c70d630c c70dbe3c c70dbe20 c01ce43c c0191a44
be20: c01c9c48 c704a800 00000041 00001043 c70dbe5c c70dbe40 c01cc63c c01ce388
be40: 00000001 00000000 c70dbe78 c70d6300 c70dbec4 c70dbe60 c0210fcc c01cc5b4
be60: 00008914 00000000 30687465 00000000 00000000 00000000 001b1043 001b46a4
be80: 001b4708 001b4740 001b1043 001b46a4 001b4708 001b4740 001b4708 c66ddd80
bea0: 00008914 bee95950 c66ddd80 00000003 c70da000 0019273c c70dbed4 c70dbec8
bec0: c0211a6c c0210d18 c70dbef4 c70dbed8 c01bdab4 c02119bc c66ddd80 c66ddd80
bee0: bee95950 00008914 c70dbf14 c70dbef8 c00a1eb4 c01bd8dc c70dbf1c
c66ddd80
bf00: c6d9e028 bee95950 c70dbf7c c70dbf18 c00a2558 c00a1e8c c01bc0d0 c0095a68
bf20: c0262488 c0034c18 c6d9e000 00000000 c70dbf5c c70dbf40 c0092808 c0034c18
bf40: 00000000 00000003 c6d9e000 00000119 c70dbf84 c70dbf60 c01bc16c 00000003
bf60: bee95950 00008914 c0027fe4 c70da000 c70dbfa4 c70dbf80 c00a25f8 c00a2018
bf80: c01bcab0 00000000 00192574 00000004 00000000 00000036 00000000 c70dbfa8
bfa0: c0027e60 c00a25c8 00192574 00000004 00000003 00008914 bee95950 00192574
bfc0: 00192574 00000004 00000000 00000036 00000000 0000005c 0019273c bee95950
bfe0: bee95ebc bee95928 0000b75c 0000903c 20000010 00000003 cf68a77a 3fd5190e
Backtrace:
[<c002b390>] (__bug+0x0/0x2c) from [<c0191e24>] (emac_dev_open+0x3f0/0xc50)
[<c0191a34>] (emac_dev_open+0x0/0xc50) from [<c01ce43c>] (dev_open+0xc4/0x128)
[<c01ce378>] (dev_open+0x0/0x128) from [<c01cc63c>] (dev_change_flags+0x98/0x170)
r6:00001043 r5:00000041
r4:c704a800
[<c01cc5a4>] (dev_change_flags+0x0/0x170) from [<c0210fcc>] (devinet_ioctl+0x2c4)
r7:c70d6300 r6:c70dbe78 r5:00000000 r4:00000001
[<c0210d08>] (devinet_ioctl+0x0/0x6b0) from [<c0211a6c>] (inet_ioctl+0xc0/0xf0)
[<c02119ac>] (inet_ioctl+0x0/0xf0) from [<c01bdab4>] (sock_ioctl+0x1e8/0x248)
[<c01bd8cc>] (sock_ioctl+0x0/0x248) from [<c00a1eb4>] (vfs_ioctl+0x38/0x98)
r6:00008914 r5:bee95950 r4:c66ddd80
[<c00a1e7c>] (vfs_ioctl+0x0/0x98) from [<c00a2558>] (do_vfs_ioctl+0x550/0x5b0)
r6:bee95950 r5:c6d9e028 r4:c66ddd80
[<c00a2008>] (do_vfs_ioctl+0x0/0x5b0) from [<c00a25f8>] (sys_ioctl+0x40/0x64)
r9:c70da000 r8:c0027fe4 r6:00008914 r5:bee95950
r4:00000003
[<c00a25b8>] (sys_ioctl+0x0/0x64) from [<c0027e60>] (ret_fast_syscall+0x0/0x2c)
r7:00000036 r6:00000000 r5:00000004 r4:00192574
Code: e1a01000 e59f000c eb004704 e3a03000 (e5833000)
---[ end trace fd18f3f6111d678d
]---
Segmentation fault
when
i do ifconfig eth0 up first tym it displays the first message.if i do
it again displays the second message device busy.if do it third time it
says bug in kernel as shown in the above log can anyone tell how to
resolve this issue.the second time it says device or resource busy.I don't know why it is saying so.
I am able to use the ethernet from u-boot and able to download the kernel image and the file system image to ram using it.Anyone knw what is this problem.
with regard's
Rohan Tabish