Part Number: DLPC6401
Tool/software: Linux
Hi there,
I'm trying to communicate with the DLPC6401 using the i2c-tools on Linux.
I can scan the i2c line and detect the device at address 0x1a (0x34 >> 1).
What I'd like to do is a Long Axis Image Flip. In the datasheet, it corresponds to the register 0x08.
To flip the screen, I've tried the following: i2cset -y 1 0x1a 0x08 0x01
But the command seems to be ignored..
Any clue?
Kind regards,