This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to build `dsplib64plus.lib` on Linux?

I'm hoping that it probably doesn't matter if I use the included `dsplib64plus.lib` or if I build dsplib myself, but I want to build it myself to be sure that it's being built and compatible with the same toolchain that I'm using for the rest of my development.

I'm using a OpenEmbedded for which there appears to be an official TI package (in org.openembedded.dev/recipes/ti/ti-dsplib), but it appears that the package is just a stub (it doesn't install anything).

So how do I build `dsplib` in Linux? Particularly I'm looking for a `Makefile` or a script to convert `.pjt`s to `Makefile`s.

 

And if it doesn't matter which toolchain it's built with, then why are there instructions for rebuilding it in Windows?