This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8148: MJPEG Encoding

Part Number: TMS320DM8148


Hi,

I have following queries regarding MJPEG Encoding supported in DM8148.

1. Will 8148 MJPEG codec does encoding as per JPEG 2000 standard ?

2. If we give PAL video for MJPEG Compression, each jpeg image will be of a field or frame ? As PAL is a interlaced format, will encoder encodes it in field format or frame format

3. Can I encode a PAL video as MJPEG. Will the encoder is capable of encoding all frames/fields

4. If encoder supprots, after encoding the JPEG images will be transferred to HOST link and written to file. Will ARM is capable of writing all the frames ? Is the speed of ARM is enough to write JPEG encoded images into the file at the rate of PAL frame rate

Regards,

Pranay kumar

  • Hi Pranay,

    kashetty pranay kumar said:
    1. Will 8148 MJPEG codec does encoding as per JPEG 2000 standard ?

    No. JPEG 2000 Standard is not supported by TI MJPEG Encoder.

    kashetty pranay kumar said:
    2. If we give PAL video for MJPEG Compression, each jpeg image will be of a field or frame ? As PAL is a interlaced format, will encoder encodes it in field format or frame format

    Interlaced encoding is not supported.

    kashetty pranay kumar said:
    3. Can I encode a PAL video as MJPEG. Will the encoder is capable of encoding all frames/fields

    The supported formats are listed in User guide. Please refer user-guide.

    kashetty pranay kumar said:
    4. If encoder supprots, after encoding the JPEG images will be transferred to HOST link and written to file. Will ARM is capable of writing all the frames ? Is the speed of ARM is enough to write JPEG encoded images into the file at the rate of PAL frame rate

    1080p60 is possible. Please refer datasheet for the details.

  • Pranay,

    If last reply has answered your query please close the thread.