Part Number: TMDXIDK5718
Hi
Im using an AM571x IDK eval board and wants to run the profinet example with an ABB PLC.
It is possible scan the profinet chain. Then I see a device with name “molex-devti”. I can assign an ip address, start/stop led signaling (D16 / Industrial LED 0 à green blinking) or assign an IO-device name.
Then I set up the device with the gsd file. but I only see a blinking green LED (changes from blue blinking to green) D17 / Industrial LED1.
The plc diagnostics says that node is inactive. I get the following diagnostic state:
“The IO-Device reported a ModuleDiffBlock during connection establishment”
Before I compiled the example, I patched the pdk with the files in folder “protocols\pdk_patches\03.03.00” and did a new build of the pdk (gmake).
For me it looks that the gsd file (details see below) does not match to the example.
CCS: CCS7.0.0.00043
SDK: ti-processor-sdk-rtos-am57xx-evm-03.03.00.04
IDK: PRU-ICSS-Profinet_Slave_01.00.01.00
PLC: ABB PM590 with CM579 (Profinet Master)
Eval-Board: AM571x Industrial Development Kit (TMDXIDK5718)
Example: profinet_slave_AM571x_arm
GSD: GSDML-V2.32-MOLEX_TI-AM57xxProfinet_SDK-20160113.xml
Best regards
Christoph