Dear all,
How is the DVEVM boards MAC address set in the DM365 DVEVM? Is it simply a uBoot environment setting? Is it pulled from hardware during the uBoot bootup sequence? The only approach I have in mind at the moment is querying a MAC EEPROM (SPI or I2C - both are available) to ensure our MAC's are unique but I am not too sure whether this is the best way forward.
I would really would appreciate someone giving me a a nudge in the right direction as to the most practical solution (even if it does not involve an external MAC eeprom) & some pointers.
Many thanks,
NickA