Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138, WL1831
Tool/software: Linux
Hello, we intend to use the OMAPL138 processor to run the embedded Linux system, then use the WL1831 module's Bluetooth function through the processor. But because of the beginning of studying with these things, we encountered some of the following questions:
1, when installed Processor SDK on the computer runs linux system, the OMAPL138 processor does not find the corresponding Processor SDK but only MCSDK; Will jutst only installation of this MCSDK software can use WL1831 module's Bluetooth function?
2, according to the Wiki page on the WL18xx Bluetooth protocol stack description, there need to create an SD card; but in accordance with the steps, we do not find create-sdcard.sh this file in the MCSDK software path. So we can not continue the corresponding operation.
3, Wiki page on the WL1831 module is all about the AM335 EVM, there is no description of the OMAPL138 processor; so we want to know that if use the OMAPL138 processor to development WL1831 module , is not the same with the AM335 EVM steps?
4, the process to develop WL1831 module Bluetooth function : in the Linux system computer to install the SDK software, and then call the function of the program, and then generate executable files; Finally, the executable file in the OMAPL138 processor to run to get result. is this ok?
thanks.