This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/OMAP-L138: Problem when Loading the EVM GEL file : OMAP-L138 Preparing SD Card for Boot

Part Number: OMAP-L138

Tool/software: Linux

Hi , I have bought OMAP-L138 LCDK for my company and I have some questions:

1) Which target configuration file must I use ?

2) Can I boot and emulator without SD-Card ? If can , how can I do ? 

2) SD card attached with the box was broken, I want use my SD card for boot and follow this link : processors.wiki.ti.com/index.php/OMAP-L138_Preparing_SD_Card_for_Boot

I use CCS v5.4 and I don't know how can I load the EVM file   and connect to the ARM core  and Load the SDMMCWriter_ARM(DSP).out and run. 

Please help me !!! Thanks !!!