Other Parts Discussed in Thread: CCSTUDIO
I use bios_5_31_02, codec_engine_2_24_01, dsplink_1_63, xdctools_3_15_00_50, xdais_6_24
to compile DSP server in windows, but when I use "xdc release -PR ." to create X64P file,
I get link error messages,
C:\CCStudio_v3.3\codec_engine_2_24_01\packages\ti\sdo\ce\VIDENCCOPY_server>xdc r
elease -PR .
making release: Tue Sep 1 13:28:32 2009 ...
======== .interfaces [.] ========
making package.mak (because of package.bld) ...
building for target C64P ...
generating interfaces for package ti.sdo.ce.VIDENCCOPY_server (because package/p
ackage.xdc.inc is older than package.xdc) ...
.interfaces files complete: Tue Sep 1 13:28:48 2009.
======== .libraries [.] ========
.libraries files complete: Tue Sep 1 13:28:49 2009.
======== .dlls [.] ========
.dlls files complete: Tue Sep 1 13:28:50 2009.
======== .executables [.] ========
configuring VIDENCCOPY_server.x64P from package/cfg/VIDENCCOPY_server_x64P.cfg .
..
platform = ti.platforms.evmDM6446
Warning: ti.sdo.ce.VIDENCCOPY.ce.VIDENCCOPY did not supply a max DARAM scratch s
ize; assuming 0 bytes is sufficient.
Warning: ti.sdo.ce.VIDENCCOPY.ce.VIDENCCOPY did not supply a max SARAM scratch s
ize; assuming 0 bytes is sufficient.
ti.sdo.ce.ipc.bios.close(): loading dsplink.dsp
NOTE: You can find the complete server data sheet in ./package/info/VIDENCCOPY_s
erver.x64P.DataSheet.html
--------------------------------------------------------------------------------
-------------------------
Warning: incompatible use of package 'ti.bios' [in C:/CCStudio_v3.3/bios_5_31_02
/packages/ti/bios/]: version of the loaded package 'ti.bios' is [5, 2, 3, 14], w
hile 'ti.sdo.ce.bioslog' [in C:/CCStudio_v3.3/codec_engine_2_24_01/packages/ti/s
do/ce/bioslog/] was built with 'ti.bios' [5, 2, 5, 12], while 'ti.sdo.fc.dskt2'
[in C:/CCStudio_v3.3/codec_engine_2_24_01/cetools/packages/ti/sdo/fc/dskt2/] was
built with 'ti.bios' [5, 2, 5, 12], while 'ti.sdo.fc.dman3' [in C:/CCStudio_v3.
3/codec_engine_2_24_01/cetools/packages/ti/sdo/fc/dman3/] was built with 'ti.bio
s' [5, 2, 5, 12], while 'ti.sdo.ce.ipc.bios' [in C:/CCStudio_v3.3/codec_engine_2
_24_01/packages/ti/sdo/ce/ipc/bios/] was built with 'ti.bios' [5, 2, 5, 12], whi
le 'ti.sdo.fc.acpy3' [in C:/CCStudio_v3.3/codec_engine_2_24_01/cetools/packages/
ti/sdo/fc/acpy3/] was built with 'ti.bios' [5, 2, 5, 12], while 'ti.sdo.fc.memut
ils' [in C:/CCStudio_v3.3/codec_engine_2_24_01/cetools/packages/ti/sdo/fc/memuti
ls/] was built with 'ti.bios' [5, 2, 5, 12], while 'ti.sdo.ce.osal.bios' [in C:/
CCStudio_v3.3/codec_engine_2_24_01/packages/ti/sdo/ce/osal/bios/] was built with
'ti.bios' [5, 2, 5, 12], while 'ti.bios.utils' [in C:/CCStudio_v3.3/codec_engin
e_2_24_01/cetools/packages/ti/bios/utils/] was built with 'ti.bios' [5, 2, 5, 12
]
will link with ti.sdo.ce.video:lib/release/video.a64P
will link with ti.sdo.ce.bioslog:lib/release/bioslog.a64P
will link with ti.sdo.ce:lib/release/ce.a64P
will link with ti.sdo.ce.alg:lib/release/Algorithm_BIOS.a64P
will link with ti.sdo.ce.ipc.bios:lib/release/ipc_bios.a64P
will link with ti.sdo.ce.osal.bios:lib/osal_bios.a64P
will link with ti.sdo.ce.osal.bios:lib/osal_bios_load.a64P
will link with ti.bios.utils:lib/utils.a64P
will link with ti.sdo.fc.acpy3:lib/release/acpy3.a64P
will link with ti.sdo.fc.memutils:lib/release/memutils.a64P
will link with ti.sdo.ce.utils.xdm:lib/release/XdmUtils.a64P
will link with ti.sdo.ce.node:lib/release/node.a64P
will link with ti.sdo.fc.dman3:lib/release/dman3Cfg.a64P
will link with ti.sdo.fc.dskt2:lib/release/dskt2.a64P
will link with ti.sdo.utils.trace:lib/release/gt.a64P
will link with ti.sdo.ce.VIDENCCOPY:lib/videnc_copy_dma.a64P
cl64P main.c ...
cl64P package/cfg/VIDENCCOPY_server_x64P.c ...
cl64P package/cfg/VIDENCCOPY_server_x64Pcfg_c.c ...
asm64P package/cfg/VIDENCCOPY_server_x64Pcfg.s62 ...
lnk64P VIDENCCOPY_server.x64P ...
undefined first referenced
symbol in file
--------- ----------------
_HWI_D_inhwi C:\CCStudio_v3.3\codec_engine_2_24_01\packages\
ti\sdo\ce\osal\bios\lib\osal_bios.a64P
_SWI_D_inswi C:\CCStudio_v3.3\codec_engine_2_24_01\packages\
ti\sdo\ce\osal\bios\lib\osal_bios.a64P
_MEM_getBaseAddress C:\CCStudio_v3.3\codec_engine_2_24_01\packages\
ti\sdo\ce\osal\bios\lib\osal_bios.a64P
>> error: symbol referencing errors - 'VIDENCCOPY_server.x64P' not built
gmake[1]: *** [VIDENCCOPY_server.x64P] Error 1
xdctools_3_15_00_50\gmake.exe: *** [.,.executables] Error 2
which lib include HWI_D_inhwi, SWI_D_inswi and MEM_getBaseAddress? how to link the X64P
file correcttly? Thanks.