UBL is version 1.5, uboot is 1.3.4 ,kernel is montavista 2.6.10.
now dm355 boots ok, and i can use nand command in u-boot, but kernel cannot find the nand device:
///////
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND:nand_maf_id=0x0,nand_dev_id=0x0
No NAND device found!!!
nand_davinci nand_davinci.0: no nand device detected
......
sometimes it found maf_id and dev_id are the same :0xec, actually device id is 0xF1. How could this happen?
my nand part is K9F1G08U0C-PCB0.