Part Number: DRA744
Tool/software: Linux
Hi,
I'm using the VIP block to acquire images from multiple cameras, using a custom application based on TI's dmabuftest.
Sometimes one of the acqusitions does not start (while the others work fine). Debugging the issue, I discovered that the application hangs at VIDIOC_DQBUF ioctl, waiting indefinitely for a buffer to arrive. This happens on K4.4 both with the latest version of the VIP driver (processor-sdk-linux-automotive-3.02.00.03) and with older ones (for example processor-sdk-linux-automotive-3.00.00.03).
In kernel 3.14 it just worked fine.
Please note that this happens with multiple models of cameras, both with discrete and embedded sync signals.
Any help will be appreciated.
Regards,
Francesco