Part Number: AM5718
Other Parts Discussed in Thread: AM5728
Hello. Does LCD AM57x IDK LCD Kit is suitable for AM571x IDK EVM (not AM572x IDK EVM)?
If NO, advice one please.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thanks.
My question was because of description on
:
Description
The AM57x industrial development kit (IDK) LCD screen can be used with AM57x IDKs to add touch and display functions for the evaluation of HMI, Panel PC, and other use cases requiring high resolution displays. The AM57x IDK LCD Screen is a 10.1" display with 1080p resolution (1920x1200) and supports 10 point capacitive touch. The LCD screen is supported on the AM57x IDK (TMDXIDK5728) with Processor-SDK-Linux-RT.