Part Number: AM3352
Hi,
We are using AM3352BZCZA100 processor with TPS65217CRSLT PMIC.We want to implement RTC using battery backup from CR2032 coin cell.The output of the battery is connected directly to the VDDS_RTC(D7) pin of AM3352 processor.
1) Can this only battery power(1.8V) to VDDS_RTC pin is enough to run processor in RTC only mode and enable internal RTC ?
2) Is there any delay during swtching off processor from normal operation mode to RTC only mode ie, Main power switched off and only battery backup of 1.8V is provided to VDDS_RTC(D7) pin of AM3352 processor ?
3) In case any delay is there, that delay time also required to be taken into account for calculating current time using RTC ?
Thanks & regards
Manjunath.B