This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Issue on development setup GP EVM AM5728

Part Number: AM5728
Other Parts Discussed in Thread: PMP

Tool/software: Linux

Pretty new to linux and am having trouble getting an environment setup.

All has worked well in the Wiki getting started guide up until getting the EVM to boot from NFS. I was previously able to get this working under the 3.00 release but had to step away from the project for a while. As of right now when booting after running the ./setup.sh step I get the following output:

U-Boot SPL 2017.01-g9fd60700db (Jun 28 2017 - 19:55:57)
DRA752-GP ES2.0
Trying to boot from MMC1
reading uboot.env
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img


U-Boot 2017.01-g9fd60700db (Jun 28 2017 - 19:55:57 -0400)

CPU  : DRA752-GP ES2.0
Model: TI AM572x EVM Rev A3
Board: AM572x EVM REV A.3A
DRAM:  2 GiB
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
SCSI:  SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:   cpsw
Hit any key to stop autoboot:  0
switch to partitions #0, OK
mmc0 is current device
reading uEnv.txt
574 bytes read in 4 ms (139.6 KiB/s)
Importing environment from mmc0 ...
cpsw Waiting for PHY auto negotiation to complete.. done
link up on port 0, speed 1000, full duplex
BOOTP broadcast 1
BOOTP broadcast 2
BOOTP broadcast 3
BOOTP broadcast 4
BOOTP broadcast 5
BOOTP broadcast 6
BOOTP broadcast 7
BOOTP broadcast 8
BOOTP broadcast 9
BOOTP broadcast 10
BOOTP broadcast 11
BOOTP broadcast 12
BOOTP broadcast 13
BOOTP broadcast 14
BOOTP broadcast 15
BOOTP broadcast 16
BOOTP broadcast 17
BOOTP broadcast 18
BOOTP broadcast 19
BOOTP broadcast 20
BOOTP broadcast 21
BOOTP broadcast 22
BOOTP broadcast 23
BOOTP broadcast 24
BOOTP broadcast 25
BOOTP broadcast 26
BOOTP broadcast 27
BOOTP broadcast 28
BOOTP broadcast 29

Retry time exceeded; starting again
link up on port 0, speed 1000, full duplex
*** ERROR: `ipaddr' not set
link up on port 0, speed 1000, full duplex
*** ERROR: `ipaddr' not set

I am running off of a clean Ubunutu 16.04 LTS and have only tried to recreate the environment i previously had working. Im sure there is a simple fix and im guessing it is to set the IP Addr. How do I do that? Also is there any more problems I am like to have? SDK is the current 4.00.00.4 Linux SDK.

Best Regards,

Trip