This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Messy output after "booting the kernel."



When use bootm, everything works well till after having message "booting the kernel". Messy outputs displayed. 

I do not think it's because of minicom or tera term since both gave messy output at the same position. 

Any idea with this? 

  • It sounds like the console settings are not correct in u-boot.  Could you please post your entire u-boot environment variables?  Type "printenv" at the u-boot prompt.

    The console settings should be:

    console=ttyS0, 115200n8

    and this should used as part of the bootargs which is passed to the kernel

    Greg

  • Greg,

    I set the console=ttyS2, 115200n8, but I changed it as you said. 

    The console gives no information after "booting the kernal".

    ==============

    TFTP from server 192.168.0.1; our IP address is 192.168.0.5
    Filename 'uImage'.
    Load address: 0xc0700000
    Loading: #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             ############################
    done
    Bytes transferred = 1804376 (1b8858 hex)
    U-Boot > bootm
    ## Booting kernel from Legacy Image at c0700000 ...
       Image Name:   Linux-2.6.18_pro500-da830_omapl1
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1804312 Bytes =  1.7 MB
       Load Address: c0008000
       Entry Point:  c0008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.............................................................
    ........................................................... done, booting the ke
    rnel.


    U-Boot 1.3.3 (Apr 23 2009 - 17:32:00)

    I2C:   ready
    DRAM:  64 MB
    In:    serial
    Out:   serial
    Err:   serial
    ARM Clock : 300000000 Hz
    More than one PHY detected.
    Hit any key to stop autoboot:  0
    U-Boot > printenv
    bootdelay=3
    baudrate=115200
    ethaddr=00:0e:99:02:fd:04
    autoload=no
    nfshost=192.168.0.1
    autoboot=no
    mem=32M
    bootcmd=dhcp;tftp
    rootpath=/home/MECHENG/guo.132/workdir/filesys
    bootfile=uImage
    filesize=1B8858
    fileaddr=C0700000
    netmask=255.255.255.0
    ipaddr=192.168.0.5
    serverip=192.168.0.1
    dnsip=192.168.0.1
    bootarfs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=dev/nfs nfsboot=192.168
    .0.1://home/MECHENG/guo.132/workdir/filesysy, nolock mem=32M
    bootargs=console=ttyS0, 115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=192.1
    68.0.1:/home/MECHENG/guo.132/workdir/filesys, nolock mem=32M
    stdin=serial
    stdout=serial
    stderr=serial
    ver=U-Boot 1.3.3 (Apr 23 2009 - 17:32:00)

    Environment size: 666/16380 bytes
    U-Boot > dhcp
    BOOTP broadcast 1
    *** Unhandled DHCP Option in OFFER/ACK: 28
    *** Unhandled DHCP Option in OFFER/ACK: 28
    DHCP client bound to address 192.168.0.5
    U-Boot > tftp
    TFTP from server 192.168.0.1; our IP address is 192.168.0.5
    Filename 'uImage'.
    Load address: 0xc0700000
    Loading: #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             ############################
    done
    Bytes transferred = 1804376 (1b8858 hex)
    U-Boot > bootm
    ## Booting kernel from Legacy Image at c0700000 ...
       Image Name:   Linux-2.6.18_pro500-da830_omapl1
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    1804312 Bytes =  1.7 MB
       Load Address: c0008000
       Entry Point:  c0008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.............................................................
    ........................................................... done, booting the ke
    rnel.

  • If you are using a Logic PD board with OMAPL1x, then using ttyS2 in the console parameter is correct.  I apologize for the confusion because I gave you the ttyS0 setting that is correct for the OMAP3 EVM.  So you should change back to ttyS2.

    Since you said the symptom is a "messy" output I thought that the problem was the speed part of the console setting which should be 115200n8.

    I see a space in bootargs in the definition of console.  There is a space between the comma and the numerical value 115200.  Take out that space and try again with ttyS2.

    Greg

  • Greg,

    Thanks for your suggestions.

    I changed back to "ttyS2".

    The second suggestion worked. There should be no space between "console=ttyS2,115200n8" and the people who has such kind of problem should have a try of such examination.

    Cheers!