Part Number: OMAP3530
Tool/software: Linux
Hello,
I try to disable debug uart peripheral.
Using CM register it is very easy to be disabled.
But trying to use PRM register can't seem to work.
I though that CM are "on" only if the PRM which provide the power is also "on" , i.e. specific PRM activates specific CM , Right ?
If yes , than why I can't disable peripheral with PRM ?
Thank you,
Ran