Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3359, AMIC110, SYSBIOS, TLK110, TLK105L
Hello,
I have built the ethercat_slave_full_AM335x_arm project and flashed on the AM3359 Sitara ICE v2 board. The application is running fine when I connect the device to TwinCAT. I am able to connect and update the TxPDO & RxPDO data.
But when I connect the same slave device(AM335x based) with EC engineer tool(for Acontis master stack), it is not able to detect the slave device. I get following log in EC Engineer:
INF | 2017-07-10 19:06:36 | Network scan successful - 0 slaves found
INF | 2017-07-10 19:06:34 | Network scan successful - 0 slaves found
INF | 2017-07-10 19:06:30 | Network scan successful - 0 slaves found
INF | 2017-07-10 19:06:28 | Network scan successful - 0 slaves found
Do we need to do any configuration change for using the slave with Aontis master stack. I want to do this to test the EtherCAT® Master Reference Design where it is asked to generate the ENI file after scanning the network. But it is not able to scan. Reference: www.ti.com/.../tiduaf8a.pdf
regards
Mohit