Part Number: PROCESSOR-SDK-DRA7X
Other Parts Discussed in Thread: DRA742, PMP, DRA752, TVP5158
Tool/software: Linux
Hello all,
I am trying to access EVEs present on Jacinto6 platform. For this purpose, I built IPU2 xem binary using VSDK and used this IPU2 xem instead of the default IPU2 xem present on the PSDKLA image. But the memory map for VSDK and corresponding PSDKLA seems to be different and hence I am getting IVA engine open failure.
1. Is it possible to use VSDK built IPU2 xem with corresponding PSDKLA without modifications in the PSDKLA source? If not, why?
2. What are the changes needed to be done in PSDKLA source in order to be able to use the VSDK built IPU2 xem?
Used VSDK Version : VISION_SDK_02_12_02_00
Used PSDKLA Version : 3.02.00.03