This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM335X: No debug output with RTC disabled

Part Number: PROCESSOR-SDK-AM335X


Hi.

I am modifying the am335x starter kit hardware and SDK kernel, to not use RTC.

I disabled RTC in device tree and kernel config.

There is no print referring to RTC on the boot log.

When modifying the hardware as suggested, the linux stop booting if I connect RTC_PWRONRSTn to ground.

I did the modifications as suggested: http://processors.wiki.ti.com/index.php/AM335x_Schematic_Checklist#RTC

But if I connect RTC_PWRONRSTn to gnd and not 1.8V, then I get no print on the serial.

Does this suggest that something is still trying to use RTC?

Kind regards,

Ugnius