Part Number: 66AK2G02
Tool/software: Linux
My program on K2G uses both DSP and ARM with the IPC module for communications. The DSP has to start first, then the ARM. Both processors run TI RTOS, but this is a question about U-Boot. I want to use u-boot to load the images for various reasons. Loading the ARM image is straight forward.
I'm using the 2017.1 version of ti-u-boot. I see that there is an "rproc load" command, but it wants to have a binary image of the DSP code. I see that there is a tool, C:\ti\ccsv6\utils\tiobj2bin\tiobj2bin.bat that might be able to make a bin file. Is that the recommended tool?
I see there is also a "bootelf" command. Since it starts the ARM, it's not appropriate for the DSP. But it seems that this would be best. Wouldn't it be best to have an "rproc loadelf" command?
Is anyone else loading up such a two part program from uboot? Any recommendations before I dive in?