Part Number: AM4377
Tool/software: TI-RTOS
Hi, I'm using the following platform
Board : custom(DDR-less, modified from IDK.)
Application : Based on EtherCAT full feature + motor_control (in SYS/BIOS_IND_SDK_2.1.3.2)
Build profile : L3 build (mentioned in SPRAC45)
I've tried to use FoE on my board, but the example code has this defined condition.
--------------------------------------------------------------------------------------------------------------------------------
#if !defined (EXEC_FROM_IRAM) && !defined (XIP_NOR)
---------------------------------------------------------------------------------------------------------(from tiescbsp.c)
I think it means I couldn't use Flash writing in "L3 build", so I have a question.
Why can't I use flash writing in "L3 build"? I ignored that condition, but it's not working.
Is there something that I could use FoE in "L3 build"?
Thank you.