Hi Guys,
The Table 7-8 in data sheet(sprs932e for 66ak2g02) of K2G indicates the minimum of DDR3L device HS bypass capacitor total capacitance is 0.85uF. But K2G EVM only has thirteen 0.01uF HS bypass caps. (K2G EVM does have one 22uF bulk cap to meet the requirement of bulk capacitors listed in Table 7-7).
I have the following questions:
Q1: Why K2G EVM doesn’t fail the power distribution network analysis? Please see the “4 Conclusion” in sprac38, “66AK2G0x General-Purpose EVM Power Distribution Network Analysis.”
Q2: I know the capacitance requirement varies from design to design. Should I start with the same bypass capacitance on EVM? Or change it to meet the requirement listed in data sheet?
Thanks,
Brian