I need to perform a signal integrity analysis of a design with Altium Designer (17.0.9) including an AM5728 processor.
When I try to import the simulation file AM572.ibs, Rev. 1.3.4 there are a couple of errors:
1. the tool is reporting an error about the letters of the file name (fixed by using lowercase letters)
2. the tool is reporting for some lines that the lenght is exceeded (truncation to 71 characters) fixed by deleting of some characters
3. after (1.+2.) the import runs to some point where the tool crashes with an access violation. I try to validate the file with another tool (IBIS validator by IOmeth ) and this tool crashes as well so there seems to be an issue with the file?