This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

i need this file: hal_userled_dm6437.lib

this is about dm6437 connection with pc ues ndk 2.0

i need this lib file: hal_userled_dm6437.lib

if anyone has it , could you please send it to me ?

my email is jianjia321@yahoo.com.cn

can anyone tell me what is this lib file for?

  • GU MO said:

    this is about dm6437 connection with pc ues ndk 2.0

    i need this lib file: hal_userled_dm6437.lib

    if anyone has it , could you please send it to me ?

    While I am not sure about NDK 2.0, the NDK 1.92 that is included with the DM6437 EVM includes this file in C:\dvsdk_1_11_00_00\ndk_1_92_00_22_eval\packages\ti\ndk\lib\hal\evmdm6437, the DVSDK that has this can be obtained after registering a DM6437 EVM board through www.ti.com/davinciregistration. I have not used NDK 2.0 on the DM6437 myself, but I took a look at the NDK 2.0 install and I do not see the file either, are you looking for this file due to some build error?

    GU MO said:
    can anyone tell me what is this lib file for?

    This would be a hardware abstraction layer library for the LEDs on the DM6437 EVM board, kind of like a LED software driver.