Other Parts Discussed in Thread: DP83848C, AM3352, TPS65910
Tool/software: Linux
Hi,
I am using TI Sitara PSP having Linux version v4.4.41. I am porting Linux on my custom board. I ported linux v3.2 successfully on it bur due to unavailability of some required drivers I have decided to use linux v4.4.41.
in that I modified uboot for custom board, It loads a linux kernel. currently I am facing one issue I am booting from sd card but linux kernel hangs at
"Waiting for root device /dev/mmcblk0p2...". I also searched on e2e community regarding a same problem but it could'nt solved a problem.
So Please guide me where I am wrong,
following is my kernel log
U-Boot SPL 2017.03 (Apr 20 2017 - 12:01:49)
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
Trying to boot from MMC1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
reading u-boot.img
reading u-boot.img
U-Boot 2017.03 (Apr 20 2017 - 12:01:49 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
DRAM: 256 MiB
NAND: 1024 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
ERROR: No USB device found
at drivers/usb/gadget/ether.c:2709/usb_ether_init()
<ethaddr> not set. Validating first E-fuse MAC
Net: Could not get PHY for ethernet@4a100000: addr 0
eth0: ethernet@4a100000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
206 bytes read in 5 ms (40 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
Running uenvcmd ...
reading uImage
3466928 bytes read in 378 ms (8.7 MiB/s)
reading am335x-evm.dtb
42154 bytes read in 12 ms (3.3 MiB/s)
## Booting kernel from Legacy Image at 80007fc0 ...
Image Name: Linux-4.4.41-gf9f6f0db2d
Created: 2017-07-06 13:47:04 UTC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3466864 Bytes = 3.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
## Flattened Device Tree blob at 80f80000
Booting using the fdt blob at 0x80f80000
XIP Kernel Image ... OK
Loading Device Tree to 8df1e000, end 8df2b4a9 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.41-gf9f6f0db2d (root@linuxadmin-admin) (gcc version 4.9.2 20140904 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.09 - Linaro GCC 4.9-2014.09) ) #1 PREEMPT Thu Jul 6 19:16:33 IST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 mem=256M rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 200348K/262144K available (6595K kernel code, 317K rwdata, 2344K rodata, 264K init, 265K bss, 12644K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08c3034 (8941 kB)
[ 0.000000] .init : 0xc08c4000 - 0xc0906000 ( 264 kB)
[ 0.000000] .data : 0xc0906000 - 0xc09554a0 ( 318 kB)
[ 0.000000] .bss : 0xc09554a0 - 0xc0997c70 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000025] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000066] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000086] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000432] clocksource_probe: no matching clocksources found
[ 0.000748] Console: colour dummy device 80x30
[ 0.000793] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000805] This ensures that you still see kernel messages. Please
[ 0.000815] update your kernel commandline.
[ 0.000846] Calibrating delay loop... 398.13 BogoMIPS (lpj=1990656)
[ 0.048188] pid_max: default: 32768 minimum: 301
[ 0.048412] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.048433] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.049662] Initializing cgroup subsys io
[ 0.049717] Initializing cgroup subsys memory
[ 0.049781] Initializing cgroup subsys devices
[ 0.049809] Initializing cgroup subsys freezer
[ 0.049837] Initializing cgroup subsys perf_event
[ 0.049859] Initializing cgroup subsys pids
[ 0.049912] CPU: Testing write buffer coherency: ok
[ 0.050571] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.054632] devtmpfs: initialized
[ 0.080308] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.106931] omap_hwmod: debugss: _wait_target_disable failed
[ 0.167034] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.173916] pinctrl core: initialized pinctrl subsystem
[ 0.176299] NET: Registered protocol family 16
[ 0.180693] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.208193] cpuidle: using governor ladder
[ 0.238178] cpuidle: using governor menu
[ 0.246716] OMAP GPIO hardware version 0.1
[ 0.258732] platform 44e3e000.rtc: Cannot lookup hwmod 'rtc'
[ 0.263344] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe
[ 0.269026] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.324500] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.333165] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.333270] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.333541] media: Linux media interface: v0.10
[ 0.333667] Linux video capture interface: v2.00
[ 0.333759] pps_core: LinuxPPS API ver. 1 registered
[ 0.333773] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.333844] PTP clock support registered
[ 0.333956] EDAC MC: Ver: 3.0.0
[ 0.336134] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.336794] Advanced Linux Sound Architecture Driver Initialized.
[ 0.339107] clocksource: Switched to clocksource timer1
[ 0.360313] NET: Registered protocol family 2
[ 0.361737] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.361813] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.361867] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.362015] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.362054] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.362335] NET: Registered protocol family 1
[ 0.363021] RPC: Registered named UNIX socket transport module.
[ 0.363048] RPC: Registered udp transport module.
[ 0.363060] RPC: Registered tcp transport module.
[ 0.363071] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.364677] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.368470] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.384706] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.386266] NFS: Registering the id_resolver key type
[ 0.386380] Key type id_resolver registered
[ 0.386393] Key type id_legacy registered
[ 0.386525] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.393314] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.393362] io scheduler noop registered
[ 0.393387] io scheduler deadline registered
[ 0.393722] io scheduler cfq registered (default)
[ 0.396429] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.402569] backlight supply power not found, using dummy regulator
[ 0.524722] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.532409] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.168881] console [ttyS0] enabled
[ 1.174654] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.185794] [drm] Initialized drm 1.1.0 20060810
[ 1.192760] panel panel: found backlight
[ 1.199430] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.206104] [drm] No driver support for vblank timestamp query.
[ 1.241440] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000020): FIFO underfow
[ 1.251150] Console: switching to colour frame buffer device 100x30
[ 1.255752] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.256697] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.275826] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.289350] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
[ 1.302926] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.308554] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
[ 1.319972] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.326729] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.336126] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.342904] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost
[ 1.350031] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.355943] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000104): Sync lost
[ 1.376162] loop: module loaded
[ 1.384378] libphy: Fixed MDIO Bus: probed
[ 1.449162] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.455373] davinci_mdio 4a101000.mdio: detected phy mask fdfffff7
[ 1.463702] libphy: 4a101000.mdio: probed
[ 1.467865] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver NS DP83848C 10/100 Mbps PHY
[ 1.477807] davinci_mdio 4a101000.mdio: phy[25]: device 4a101000.mdio:19, driver unknown
[ 1.487374] cpsw 4a100000.ethernet: Detected MACID = 1c:ba:8c:e6:4c:b8
[ 1.494505] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.504358] mousedev: PS/2 mouse device common for all mice
[ 1.511283] i2c /dev entries driver
[ 1.517074] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.525496] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.659283] tilcdc 4830e000.lcdc: tilcdc_crtc_irq(0x00000004): Sync lost flood detected, disabling the interrupt
[ 1.700449] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.724364] NET: Registered protocol family 10
[ 1.741422] sit: IPv6 over IPv4 tunneling driver
[ 1.747627] NET: Registered protocol family 17
[ 1.769757] Key type dns_resolver registered
[ 1.774562] omap_voltage_late_init: Voltage driver support not added
[ 1.799831] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.805425] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.822007] nand: Could not find valid ONFI parameter page; aborting
[ 1.828414] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xd3
[ 1.849118] nand: AMD/Spansion NAND 1GiB 3,3V 8-bit
[ 1.859126] nand: 1024 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.866886] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.885620] 10 ofpart partitions found on MTD device 8000000.nand
[ 1.899119] Creating 10 MTD partitions on "8000000.nand":
[ 1.909145] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.930433] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.938545] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.960331] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.968323] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.984552] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 2.000858] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 2.016464] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 2.040291] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 2.048177] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 2.109399] tps65910 0-002d: No interrupt support, no core IRQ
[ 2.128001] tps65910 0-002d: Error in configuring external control EN1
[ 2.139128] tps65910 0-002d: Failed to initialise ext control config
[ 2.159643] vrtc: failed to enable
[ 2.163351] tps65910 0-002d: failed to register tps65910-pmic regulator
[ 2.176322] tps65910-pmic: probe of tps65910-pmic failed with error -121
[ 2.189878] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 2.211812] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.218656] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 2.261961] input: volume_keys@0 as /devices/platform/volume_keys@0/input/input0
[ 2.280991] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 2.286664] hctosys: unable to open rtc device (rtc0)
[ 2.310513] vbat: disabling
[ 2.313378] lis3_reg: disabling
[ 2.316722] ALSA device list:
[ 2.329130] No soundcards found.
[ 2.349441] Waiting for root device /dev/mmcblk0p2...
waiting for your reply.
Best Regards,
Vishvajeet.