Other Parts Discussed in Thread: AMIC110
Tool/software: TI-RTOS
Hi,
We are evaluating the combination of C2000 (motion) and Sitara AM335x as the industrial communications slave for multiple protocols. The actual concept is the following:
C2000: Motion controller, SPI communications with Sitara using a "generic protocol"
Sitara: PRU with EtherCAT/PROFINET/Ethernet/IP firmware, ARM with the corresponding slave stack and translation to the SPI "generic protocol".
Some of your documents suggest to develop the application on the Sitara, which is not suitable for this case. Also, in some other documents, it is suggested to run the stack on the C2000 (which would only be usable using the AMIC110 emulating ET1100). We are afraid of obtaining poor performance with the approach detailed above (latency may be too high?).
Have you had any experiences with architectures like the one shown above? Any recommendations or IT engineers we could talk to?
Thanks,