This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4379: CPSW not able to transmit frames

Part Number: AM4379
Other Parts Discussed in Thread: TMDSIDK437X

Dear Experts,

as a preparation for our custom board I am trying to bring up th CPSW Interface on an Industrial Evaluation Module 437x Board. I studied the technical refrence manual and looked in various drivers for an example.

I only want to use Port 1 (it is the only port on the eval board) as a single MAC Port. No switch functionality is required.

My software is working so far that I can receive packets, but I can not send packets on the line. The TX-DMA is working fine. If I want to sent a packet and write the address of an descriptor to the CPSW_STATERAM_TX0_HDP register, a TX-Interrupt is issued and the descriptor Owner-Bit and EOQ-Bit are set proper. In the CPSW_DMASTS Register is no error indicated. Never the less no packet is seen on the line.


Has anyone an idea what is not correct configured ? I have attended a register dump of the CPSW registers from Code Composer Studio.

Is there any where a ready to use example program for Code Composer Studio and the TMDSIDK437X Industrial Development Kit Board ? so that I can look for the configured register values ?

Thanks for your help.

Regards, Matthias

521177 9
R CPSW_SS_CPSW_SS_ID_VER 0x0000000B 0x0019010F
R CPSW_SS_CPSW_SS_CTRL 0x0000000B 0x00000000
R CPSW_SS_CPSW_SS_SOFT_RESET 0x0000000B 0x00000000
R CPSW_SS_CPSW_SS_STAT_PORT_EN 0x0000000B 0x00000002
R CPSW_SS_CPSW_SS_PTYPE 0x0000000B 0x00000000
R CPSW_SS_CPSW_SS_SOFT_IDLE 0x0000000B 0x00000000
R CPSW_SS_CPSW_SS_THRU_RATE 0x0000000B 0x00003003
R CPSW_SS_CPSW_SS_GAP_THRESH 0x0000000B 0x0000000B
R CPSW_SS_CPSW_SS_TX_START_WDS 0x0000000B 0x00000020
R CPSW_SS_CPSW_SS_FLOW_CTRL 0x0000000F 0x0001
R CPSW_SS_CPSW_SS_VLAN_LTYPE 0x0000000B 0x81008100
R CPSW_SS_CPSW_SS_TS_LTYPE 0x0000000B 0x00000000
R CPSW_SS_CPSW_SS_DLR_LTYPE 0x0000000F 0x80E1
R CPSW_SS_CPSW_SS_STS 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_CTRL 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_MAX_BLKS 0x0000000B 0x00000104
R CPSW_PORT_CPSW_PORT_P0_BLK_CNT 0x0000000B 0x00000042
R CPSW_PORT_CPSW_PORT_P0_TX_IN_CTL 0x0000000B 0x000040C0
R CPSW_PORT_CPSW_PORT_P0_VLAN 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_TX_PRI_MAP 0x0000000B 0x33221001
R CPSW_PORT_CPSW_PORT_P0_CPDMA_TX_PRI_MAP 0x0000000B 0x76543210
R CPSW_PORT_CPSW_PORT_P0_CPDMA_RX_CH_MAP 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP0 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP1 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP2 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP3 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP4 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP5 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP6 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P0_RX_DSCP_PRI_MAP7 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_CTRL 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_TS_CTL2 0x0000000B 0x00040000
R CPSW_PORT_CPSW_PORT_P1_MAX_BLKS 0x0000000B 0x00000113
R CPSW_PORT_CPSW_PORT_P1_BLK_CNT 0x0000000B 0x00000042
R CPSW_PORT_CPSW_PORT_P1_TX_IN_CTL 0x0000000B 0x080040C0
R CPSW_PORT_CPSW_PORT_P1_VLAN 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_TX_PRI_MAP 0x0000000B 0x33221001
R CPSW_PORT_CPSW_PORT_P1_TS_SEQ_MTYPE 0x0000000B 0x001E0000
R CPSW_PORT_CPSW_PORT_P1_SA_LO 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_SA_HI 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_SEND_PERCENT 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP0 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP1 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP2 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP3 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP4 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP5 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP6 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P1_RX_DSCP_PRI_MAP7 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_CTRL 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_TS_CTL2 0x0000000B 0x00040000
R CPSW_PORT_CPSW_PORT_P2_MAX_BLKS 0x0000000B 0x00000113
R CPSW_PORT_CPSW_PORT_P2_BLK_CNT 0x0000000B 0x00000041
R CPSW_PORT_CPSW_PORT_P2_TX_IN_CTL 0x0000000B 0x080040C0
R CPSW_PORT_CPSW_PORT_P2_VLAN 0x0000000F 0x0000
R CPSW_PORT_CPSW_PORT_P2_TX_PRI_MAP 0x0000000B 0x33221001
R CPSW_PORT_CPSW_PORT_P2_TS_SEQ_MTYPE 0x0000000B 0x001E0000
R CPSW_PORT_CPSW_PORT_P2_SA_LO 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_SA_HI 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_SEND_PERCENT 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP0 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP1 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP2 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP3 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP4 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP5 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP6 0x0000000B 0x00000000
R CPSW_PORT_CPSW_PORT_P2_RX_DSCP_PRI_MAP7 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_IDVER 0x0000000B 0x00180109
R CPSW_CPDMA_CPSW_TX_CTRL 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_TX_TEARDOWN 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX_IDVER 0x0000000B 0x00180109
R CPSW_CPDMA_CPSW_RX_CTRL 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_RX_TEARDOWN 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_CPDMA_SOFT_RESET 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_DMACTRL 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_DMASTS 0x0000000B 0x80000000
R CPSW_CPDMA_CPSW_RX_BUFFER_OFFSET 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_EMCTRL 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI0_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI1_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI2_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI3_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI4_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI5_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI6_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_PRI7_RATE 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_INTSTAT_RAW 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_INTSTAT_MASKED 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_TX_INTMASK_SET 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_TX_INTMASK_CLR 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_CPDMA_IN_VECTOR 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_CPDMA_EOI_VECTOR 0x0000000B 0x00000002
R CPSW_CPDMA_CPSW_RX_INTSTAT_RAW 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX_INTSTAT_MASKED 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX_INTMASK_SET 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_RX_INTMASK_CLR 0x0000000B 0x00000001
R CPSW_CPDMA_CPSW_DMA_INTSTAT_RAW 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_DMA_INTSTAT_MASKED 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_DMA_INTMASK_SET 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_DMA_INTMASK_CLR 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX0_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX1_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX2_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX3_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX4_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX5_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX6_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX7_PENDTHRESH 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX0_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX1_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX2_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX3_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX4_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX5_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX6_FREEBUFFER 0x0000000B 0x00000000
R CPSW_CPDMA_CPSW_RX7_FREEBUFFER 0x0000000B 0x00000000
R CPSW_STATS_GOODRX 0x0000000B 0x0000000B
R CPSW_STATS_BROADCAST_RX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_MULTICAST_RX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_PAUSE_RX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_CRC_ERRORS 0x0000000B 0x00000000
R CPSW_STATS_RX_ALIGN_ERRORS 0x0000000B 0x00000000
R CPSW_STATS_OVERSIZE_RX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_JABBERS 0x0000000B 0x00000000
R CPSW_STATS_UNDERSIZE_RX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_FRAGMENTS 0x0000000B 0x00000000
R CPSW_STATS_RX_OCTETS 0x0000000B 0x000002C0
R CPSW_STATS_GOOD_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_BROADCAST_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_MULTICAST_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_PAUSE_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_DEFERRED_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_COLLISIONS 0x0000000B 0x00000000
R CPSW_STATS_SINGLE_COLLISION_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_MULTIPLE_COLLISION_TX_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_EXCESSIVE_COLLISIONS 0x0000000B 0x00000000
R CPSW_STATS_LATE_COLLISIONS 0x0000000B 0x00000000
R CPSW_STATS_TX_UNDERRUN 0x0000000B 0x00000000
R CPSW_STATS_CARRIER_SENSE_ERRORS 0x0000000B 0x00000000
R CPSW_STATS_TX_OCTETS 0x0000000B 0x00000000
R CPSW_STATS_RX_TX_64_OCTET_FRAMES 0x0000000B 0x0000000B
R CPSW_STATS_RX_TX_65_OCTET_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_TX_128_OCTET_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_TX_256_OCTET_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_TX_512_OCTET_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_RX_TX_1024_OCTET_FRAMES 0x0000000B 0x00000000
R CPSW_STATS_NET_OCTETS 0x0000000B 0x000002C0
R CPSW_STATS_RX_START_OF_FRAME_OVERRUNS 0x0000000B 0x00000000
R CPSW_STATS_RX_MIDDLE_OF_FRAME_OVERRUNS 0x0000000B 0x00000000
R CPSW_STATS_RX_DMA_OVERRUNS 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX0_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX1_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX2_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX3_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX4_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX5_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX6_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX7_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX0_HDP 0x0000000B 0x4A102EB0
R CPSW_STATERAM_CPSW_STATERAM_RX1_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX2_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX3_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX4_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX5_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX6_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX7_HDP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX0_CP 0x0000000B 0x4A103F2C
R CPSW_STATERAM_CPSW_STATERAM_TX1_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX2_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX3_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX4_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX5_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX6_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_TX7_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX0_CP 0x0000000B 0x4A102EC4
R CPSW_STATERAM_CPSW_STATERAM_RX1_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX2_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX3_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX4_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX5_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX6_CP 0x0000000B 0x00000000
R CPSW_STATERAM_CPSW_STATERAM_RX7_CP 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_IDVER 0x0000000B 0x4E8A0105
R CPSW_CPTS_CPSW_CPTS_CTRL 0x0000000B 0x00000004
R CPSW_CPTS_CPSW_RFTCLK_SEL 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_PUSH 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_LOAD_VAL 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_LOAD_EN 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_COMP_VAL 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_COMP_LENGTH 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_INTSTAT_RAW 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_INTSTAT_MASKED 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_INT_EN 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_EVT_POP 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_EVT_LOW 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_EVT_MID 0x0000000B 0x00000000
R CPSW_CPTS_CPSW_CPTS_EVT_HIGH 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_IDVER 0x0000000B 0x00290104
R CPSW_ALE_CPSW_ALE_CTRL 0x0000000B 0x80000010
R CPSW_ALE_CPSW_ALE_PRESCALE 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_UNKNOWN_VLAN 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_TBLCTL 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_TBLW2 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_TBLW1 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_TBLW0 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_0 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_1 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_2 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_3 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_4 0x0000000B 0x00000000
R CPSW_ALE_CPSW_ALE_PORTCTL_5 0x0000000B 0x00000000
R CPSW_SL1_CPSW_SL_IDVER 0x0000000B 0x00170113
R CPSW_SL1_CPSW_SL_MACCTRL 0x0000000B 0x00000021
R CPSW_SL1_CPSW_SL_MACSTS 0x0000000B 0x80000008
R CPSW_SL1_CPSW_SL_SOFT_RESET 0x0000000B 0x00000000
R CPSW_SL1_CPSW_SL_RX_MAXLEN 0x0000000B 0x000005F0
R CPSW_SL1_CPSW_SL_BOFFTEST 0x0000000B 0x02B30000
R CPSW_SL1_CPSW_SL_RX_PAUSE 0x0000000B 0x00000000
R CPSW_SL1_CPSW_SL_TX_PAUSE 0x0000000B 0x00000000
R CPSW_SL1_CPSW_SL_EMCTRL 0x0000000B 0x00000000
R CPSW_SL1_CPSW_SL_RX_PRI_MAP 0x0000000B 0x76543210
R CPSW_SL1_CPSW_SL_TX_GAP 0x0000000B 0x0000000C
R CPSW_SL2_CPSW_SL_IDVER 0x0000000B 0x00170113
R CPSW_SL2_CPSW_SL_MACCTRL 0x0000000B 0x00000000
R CPSW_SL2_CPSW_SL_MACSTS 0x0000000B 0x80000000
R CPSW_SL2_CPSW_SL_SOFT_RESET 0x0000000B 0x00000000
R CPSW_SL2_CPSW_SL_RX_MAXLEN 0x0000000B 0x000005EE
R CPSW_SL2_CPSW_SL_BOFFTEST 0x0000000B 0x00AB0000
R CPSW_SL2_CPSW_SL_RX_PAUSE 0x0000000B 0x00000000
R CPSW_SL2_CPSW_SL_TX_PAUSE 0x0000000B 0x00000000
R CPSW_SL2_CPSW_SL_EMCTRL 0x0000000B 0x00000000
R CPSW_SL2_CPSW_SL_RX_PRI_MAP 0x0000000B 0x76543210
R CPSW_SL2_CPSW_SL_TX_GAP 0x0000000B 0x0000000C
R CPSW_MDIO_MDIO_VER 0x0000000B 0x40070106
R CPSW_MDIO_MDIO_CTRL 0x0000000B 0x41040059
R CPSW_MDIO_MDIO_ALIVE 0x0000000B 0x00000001
R CPSW_MDIO_MDIO_LINK 0x0000000B 0x00000001
R CPSW_MDIO_MDIO_LINKINTRAW 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_LINKINTMASKED 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERINTRAW 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERINTMASKED 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERINTMASKSET 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERINTMASKCLR 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERACCESS0 0x0000000B 0x23E00328
R CPSW_MDIO_MDIO_USERPHYSEL0 0x0000000B 0x00000040
R CPSW_MDIO_MDIO_USERACCESS1 0x0000000B 0x00000000
R CPSW_MDIO_MDIO_USERPHYSEL1 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_IDVER 0x0000000B 0x4EDB1902
R CPSW_WR_CPSW_WR_SOFT_RESET 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_CTRL 0x0000000B 0x0000000A
R CPSW_WR_CPSW_WR_INT_CTRL 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_RX_THRESH_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_RX_EN 0x0000000B 0x00000001
R CPSW_WR_CPSW_WR_C0_TX_EN 0x0000000B 0x00000001
R CPSW_WR_CPSW_WR_C0_MISC_EN 0x0000000B 0x00000002
R CPSW_WR_CPSW_WR_C1_RX_THRESH_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_RX_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_TX_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_MISC_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_RX_THRESH_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_RX_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_TX_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_MISC_EN 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_RX_THRESH_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_RX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_TX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_MISC_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_RX_THRESH_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_RX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_TX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_MISC_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_RX_THRESH_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_RX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_TX_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_MISC_STAT 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_RX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C0_TX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_RX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C1_TX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_RX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_C2_TX_IMAX 0x0000000B 0x00000000
R CPSW_WR_CPSW_WR_RGMII_CTL 0x0000000B 0x0000000B