Hi All,
I am working on DSK5510 and want to initialize the McBSP ports on it.
McBSP1 for writing control data into the CODEC.
I do not want to use CSL/BSL for writing to the McBSP registers.
Just saw some example project dsk1_app.pjt in the example projects.
It uses the some functions to write to the McBSP registers (like DSK5510_init(), McBSP_Start()....),
basically looking to write into the McBSP peripheral registers on C5510.
I want to have source code for these functions.
Can some one please suggest me as to where I can find this source code?
Regards,
Aditi