Hi,all
In the demo of DM6437 EVM devices are added under the User-Defined Devices
in the TCF graphical configuration tool. In the application source code, the device is used via GIO
API. I see there is a item named GIO General Input/Output Manager. Why are devices added under
User-Defined Devices instead of GIO General Input/Output Manager? What is the relationship
between them?
Best Regards
Jogging