Tool/software: Linux
Hello all
I am working AM335x running on Linux 3.12.
Basically read data from OMAP UART and the problem is for every read only 1 byte is read always.
looking into omap uart driver following is the configuration
/* FIFO ENABLE, DMA MODE */
up->scr |= OMAP_UART_SCR_RX_TRIG_GRANU1_MASK;
/*
* NOTE: Setting OMAP_UART_SCR_RX_TRIG_GRANU1_MASK
* sets Enables the granularity of 1 for TRIGGER RX
* level. Along with setting RX FIFO trigger level
* to 1 (as noted below, 16 characters) and TLR[3:0]
* to zero this will result RX FIFO threshold level
* to 1 character, instead of 16 as noted in comment
* below.
*/
/* Set receive FIFO threshold to 16 characters and
* transmit FIFO threshold to 16 spaces
*/
up->fcr &= ~OMAP_UART_FCR_RX_FIFO_TRIG_MASK;
up->fcr &= ~OMAP_UART_FCR_TX_FIFO_TRIG_MASK;
up->fcr |= UART_FCR6_R_TRIGGER_16 | UART_FCR6_T_TRIGGER_24 |
UART_FCR_ENABLE_FIFO;
I tried to remove granularity it can read more then 1 but there is problem with data.
Can anybody help me to set the correct configuration to Driver