This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3359: RTC issue

Part Number: AM3359
Other Parts Discussed in Thread: TPS65910

Tool/software: Linux

Hello,i have a RTC  trouble in AM3359.

I have a custom AM3359 board.  But the RTC can not keep the time all the time .  When i use a new  Li-ion  , it can be keep almost 1~2 months,and then the cell has  the low voltage(about 2.2V ). Both the same in power off and power on condition,

Our AM3359  mark is AM3359BZCZA80. Silicon Version is PG2.0  And the PMIC is TPS65910.  The Li-ion use the Panasonic CR2032. It seems like the RTC have the high consumption or the high leak current.

The attachment file is the schematic of the  power part and the RTC part.

Anyone use the on-chip RTC in matured product? Please help me ,thanks ~~

 Pg04_ AM335X Section 3 .pdfPg05_ Power Management.pdf